When the the DSP is sending configuration to a device via the I2C bus, will I2C interrupts be generated on the A8 and the HDVPSS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When the the DSP is sending configuration to a device via the I2C bus, will I2C interrupts be generated on the A8 and the HDVPSS?
Typically interrupts from IP are mapped onto number of processors like A8, HDVPSS processor etc so that any of the processor can use the I2C based on architecture requirement. Now the interrupt needs to be enabled, on that processor, to receive it. Typically interrupt on the processor gets enabled once the software registers the interrupt with OS like "irq_request()" call being made on Linux and "Hwi_create()" for BIOS.
Regards,
Hardik Shah