This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J784S4: PROCESSOR-SDK-J784S4

Part Number: PROCESSOR-SDK-J784S4

Hello,

We are working on ti-processor-sdk-rtos-j784s4-evm-09_02_00_05 and trying to bring up MCU2_1, MCU3_0, MCU3_1, MCU_4_0, MCU4_1 cores. We have been able to build some test applications from processor SDK and wish to load the core specific firmware (example: GPIO_LedBlink_TestApp_freertos_mcu2_1_release.xer5f) on respective core.

We are currently running PSDK Linux on our A72 core and would like to explore/know the procedure to load the firmware via u-boot. Please help on this topic. Also we would like to know if  there is a possibility of loading the firmware via tiboot3. If yes, then some documentation link would be really helpful for the same.

Thanks in advance,

Srinivasan