Part Number: AM3352
Hi Support Team,
There is a problem with a customer's board using AM3352BZCZ100 that does not operate normally in 0°C environment.
It is confirmed that the power supply voltage is within the normal range under the above conditions and the CPU does not start up normally.
In addition, since this problem is reproduced when only the CPU is cooled at normal temperature with a rapid cooling sprayer,
it is certain that the CPU is the cause of the problem. In addition, when the CPU is warmed up, it starts booting normally.
The operating temperature range of AM3352BZCZ100 is 0°C to 90°C, so it is not operating normally within the operating range.
This problem occurs in 1 unit in 5 units.
If you have any idea of the cause of the above problem, could you please let us know what we can do to solve the problem?
Best Regards,
Kanae