Other Parts Discussed in Thread: TVP5146
Hi,
We wanted to capture CVBS input at CIF/QCIF resolution for some reasons.
One option is we can capture at 720x576 resolution and then resize it to target (CIF/QCIF) resolution.
We want capturing at a resolution which is configurable and display at same resolution (similar to saMmapLoopback implementation)
saMmapLoopback example fails if capture resolution is set other than 720x576.
It appears like v4l capture driver only supports 720x576 resolution. Where do we need modifications ? Please help.
We are using dvsdk_4_00_00_17 / PSP_03.00.01.06 (kernel 2.6.32) on AM3530/AM37 board.
Regards,
Avijit