The datasheet of AM389x says the state of pin "TIM5_OUT(pin H34 mmuxed with GP0[29]) " is PULL:IPD/IPD and DRIVE:L/L when and after POR. And I measured the level of this pin when POR,it's truely low. I want to config this pin as a pulse frequency detector(as input). I modified PINCCTRL204 as 0x00000010,but the level of the pin is still drive low.
So my question is how to config this pin as a input pin(use its capture mode)?