Part Number: AM625
Other Parts Discussed in Thread: UNIFLASH
Hi,
We have been using this method in the below link to do eMMC to bare-metal loading for the last 3 months, but today when we tried it is not working.
Here I am attaching the screenshot of the error. Please help me with this
(i) MCU+SDK Version 9.0 + TI PROCESSOR SDK 9.0

multistage2 emmc main.c file edit then compiled
emmc cfg file below:
#-----------------------------------------------------------------------------# # # # DEFAULT CONFIGURATION FILE TO BE USED WITH THE FLASHWRITER SCRIPT # # # #-----------------------------------------------------------------------------# # # By default this config file, # - points to pre-built flash writer, bootloader for this EVM # - The application image points to relative path of the ipc rpmsg linux application image for this EVM # - Make sure this application is built before running this script # - You can customized this config file to point to your own bootloader and/or application images # - You can use --operation=flashverify-emmc if you just want to verify the flash contents and not flash the file. # # First point to sbl_uart_uniflash_stage1 binary, which initialises DDR and receives sbl_uart_uniflash_stage2 binary --flash-writer=sbl_prebuilt/am62x-sk/sbl_uart_uniflash_stage1.release.tiimage # When sending sbl_uart_uniflash_stage2 binary make sure to flash at SOC memory offset 0x0. # Points to sbl_uart_uniflash_stage2 binary, which function's as a server to flash one or more files to eMMC --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_00_00_19/examples/drivers/boot/sbl_uart_uniflash_multistage/sbl_uart_uniflash_stage2/am62x-sk/r5fss0-0_nortos/ti-arm-clang/sbl_uart_uniflash_stage2.release.appimage --operation=flash --flash-offset=0x0 # Now send one or more files to flash or flashverify as needed. The order of sending files does not matter # When sending bootloader make sure to flash at offset 0x0. ROM expects bootloader at offset 0x0 of eMMC --file=sbl_prebuilt/am62x-sk/sbl_emmc_linux_stage1.release.tiimage --operation=flash-emmc --flash-offset=0x0 # 2nd stage bootloader is flashed at 0x80000 or to whatever offset your bootloader is configured for --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_00_00_19/examples/drivers/boot/sbl_emmc_linux_multistage/sbl_emmc_linux_stage2/am62x-sk/r5fss0-0_nortos/ti-arm-clang/sbl_emmc_linux_stage2.release.appimage --operation=flash-emmc --flash-offset=0x80000 # When sending application image, make sure to flash at offset 0x100000 (default) or to whatever offset your bootloader is configured for --file=/home/bpt/workspace_v12/gpio_led_blink_am62x-sk_m4fss0-0_freertos_ti-arm-clang/Debug/gpio_led_blink_am62x-sk_m4fss0-0_freertos_ti-arm-clang.appimage --operation=flash-emmc --flash-offset=0x100000 # HSM image is flashed at 0x800000 or to whatever offset your bootloader is configured for --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_00_00_19/tools/boot/HSMAppimageGen/board/am62x-sk/hsm.appimage --operation=flash-emmc --flash-offset=0x800000 # DM image is flashed at 0xa00000 or to whatever offset your bootloader is configured for --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_00_00_19/examples/drivers/ipc/ipc_rpmsg_echo_linux/am62x-sk/r5fss0-0_freertos/ti-arm-clang/ipc_rpmsg_echo_linux.release.appimage --operation=flash-emmc --flash-offset=0xA00000 # Linux image is flashed at 0xC00000 or to whatever offset your bootloader is configured for --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_00_00_19/tools/boot/linuxAppimageGen/board/am62x-sk/linux.appimage --operation=flash-emmc --flash-offset=0xC00000
(ii) MCU+SDK Version 9.1 + TI PROCESSOR SDK 9.0

emmc cfg file below:
#-----------------------------------------------------------------------------# # # # DEFAULT CONFIGURATION FILE TO BE USED WITH THE FLASHWRITER SCRIPT # # # #-----------------------------------------------------------------------------# # # By default this config file, # - points to pre-built flash writer, bootloader for this EVM # - The application image points to relative path of the ipc rpmsg linux application image for this EVM # - Make sure this application is built before running this script # - You can customized this config file to point to your own bootloader and/or application images # - You can use --operation=flashverify-emmc if you just want to verify the flash contents and not flash the file. # # First point to sbl_uart_uniflash_stage1 binary, which initialises DDR and receives sbl_uart_uniflash_stage2 binary --flash-writer=sbl_prebuilt/am62x-sk/sbl_uart_uniflash_stage1.release.tiimage # When sending sbl_uart_uniflash_stage2 binary make sure to flash at SOC memory offset 0x0. # Points to sbl_uart_uniflash_stage2 binary, which function's as a server to flash one or more files to eMMC --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_01_00_39/examples/drivers/boot/sbl_uart_uniflash_multistage/sbl_uart_uniflash_stage2/am62x-sk/r5fss0-0_nortos/ti-arm-clang/sbl_uart_uniflash_stage2.release.appimage --operation=flash --flash-offset=0x0 # Now send one or more files to flash or flashverify as needed. The order of sending files does not matter # When sending bootloader make sure to flash at offset 0x0. ROM expects bootloader at offset 0x0 of eMMC --file=sbl_prebuilt/am62x-sk/sbl_emmc_linux_stage1.release.tiimage --operation=flash-emmc --flash-offset=0x0 # 2nd stage bootloader is flashed at 0x80000 or to whatever offset your bootloader is configured for --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_01_00_39/examples/drivers/boot/sbl_emmc_linux_multistage/sbl_emmc_linux_stage2/am62x-sk/r5fss0-0_nortos/ti-arm-clang/sbl_emmc_linux_stage2.release.appimage --operation=flash-emmc --flash-offset=0x80000 # When sending application image, make sure to flash at offset 0x100000 (default) or to whatever offset your bootloader is configured for --file=/home/bpt/workspace_v12_5/ipc_rpmsg_echo_linux_am62x-sk_m4fss0-0_freertos_ti-arm-clang/Debug/ipc_rpmsg_echo_linux_am62x-sk_m4fss0-0_freertos_ti-arm-clang.appimage --operation=flash-emmc --flash-offset=0x100000 # HSM image is flashed at 0x800000 or to whatever offset your bootloader is configured for --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_01_00_39/tools/boot/HSMAppimageGen/board/am62x-sk/hsm.appimage --operation=flash-emmc --flash-offset=0x800000 # DM image is flashed at 0xa00000 or to whatever offset your bootloader is configured for --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_01_00_39/examples/drivers/ipc/ipc_rpmsg_echo_linux/am62x-sk/r5fss0-0_freertos/ti-arm-clang/ipc_rpmsg_echo_linux.release.appimage --operation=flash-emmc --flash-offset=0xA00000 # Linux image is flashed at 0xC00000 or to whatever offset your bootloader is configured for --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_01_00_39/tools/boot/linuxAppimageGen/board/am62x-sk/linux.appimage --operation=flash-emmc --flash-offset=0xC00000 # u-boot.img is flashed at 0x280000 --file=/home/bpt/ti/mcu_plus_sdk_am62x_09_01_00_39/tools/boot/linuxAppimageGen/board/am62x-sk/u-boot.img --operation=flash-emmc --flash-offset=0x280000
Regards,
Veerapandyan V