Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: TMDS64EVM
I am running ospi example code on default board TMDS64EVM. flash type is S28HS512T.
In TRM, it said"
12.3.2.1.2 OSPI Not Supported Features
The following features are not supported on this family of devices:
•
DMA not supported.
•
Pulse events not used.
•
In Octal-SPI and Quad-SPI mode, Mode 1, 2, and 3 are not supported.
"
However, From sdk and from example, dma is fully supported.
so in "The following features are not supported on this family of devices:", what is this family of devices? can you listed.
DMA is working fine in TMDS64EVM.
Thanks.