Hi all,
I'm doing some tests powering the system with a 180mAh single cell Li-ion battery (3.6V nominal voltage).
I've connected the positive terminal of the battery to the MAIN_BATT_IN pin of the SOM-M1 module, and the negative one to GND (in brief across C47).
When the system is on (running u-boot) and I unplug the 5V power cord, correctly the TPS65070 PMIC switches onto the battery supply and the system still remains on.
The problem arised when I tested the charging capability of the PMIC.
I read the TPS65070 PMIC is capable of charging the battery from the 5V input, but I was not able to see any charging current, even with the battery voltage as low as 2V.
Did anybody successfully charge a battery with such a system ?
Does anybody knows if there any SW/HW settings I've not considered yet ?
The Zoom™ AM1808 EVM is 1015525 Rev 2
The SOM-M1 is SOMAM1808-10-1502QHCR-A (1016966)
Best regards,
Gabriele