This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Image Processing Library for AM35xx

Other Parts Discussed in Thread: DM3730, OMAP3530

 

Hello,

 

With regards to Sitara (Cortex- A8) series.

is  there any Image Processing Library (IMGLIB)  provided for Cortex- A8 devices?

 

Regards

Mudigere

  • Mudigere,

    IMGLIB is an image processing library that has been optimized for the C64x+ DSP core but if you download the library , you will find that the library also provides an equivalent natural C code implementation of all the image library functions. You can compile and run the natural c implmentation of these function on Cortex A8. This is unlikely to give you the same performance as the DSP but it may be a good starting point for you.

    Also OMAP3530 and DM3730 is an pin compatable ARM+DSP version of AM35x and AM37x devices on which you can use the IMGLIB on the C64x+ DSP. C6EZAccel and C6EZRun tools provided in the SDKs allows ARM users access to DSP sofware . These tools can be used to run IMGLIB on the DSP from Cortex-A8 over the interprocessor communication link (DSPLINK).

    Regards,

    Rahul