Part Number: AM62P-Q1
Other Parts Discussed in Thread: SK-AM62P-LP, SYSCONFIG, AM62P
Hi guys.
We are designing a custom board based on AM62P54.
As starting reference we have used the EVM board SK-AM62P-LP
The main memory is LPDDR4 (micron MT53E512M32D1ZW-046AUT:B).
Configuring timing for the memory above is quite straight forward using SYSCONFIG DDR Subsystem Register Configuration (0.10.01).
But There are a couple of parameter which are disabled in default configuration used on evm board:
Enable Periodic WDQ leveling
Periodic ZQ calibration
On AM62P TRM or Datasheet i haven't found too much about this kind of setting and when they should be activated.
Considering this parameter involves ZQ calibration and Write leveling i suppose they should be useful if my system must function over a wide temperature range.. am i right?
As design constraints our board must function over -40° to 85° (ambient).. Should i set as active the two parameter listed above? there are drawbacks using them active?
Thanks for your reply!
Have a nicew day!