Hello,
we're in the bring up phase for our TDA4AP design. We followed for the Power supply implementation SLVUIC2 PDN 3A solution.
1) When switching on the PMIC with PMIC enable pin (ENABLE pin 20) the PMIC starts to ramp up the voltage rails and after around 10ms we also get High signals for GPIO8 and GPIO10 from the external PWRGRP Pins.
2) after around 12ms the PWRGRP signals on GPIO8, GPIO10 switch back to low and stay low.
3) From that stage the PMIC retries to enable its rails again until the rmax retry count has reached
4) We identified a higher current than expected on BUCK3 VDD_RAM_0V85 (max. 5Amp) but should be fine due to limit at 5.5A
5) We also see in the log see end of the mail that 0x5D register shows an ILIM on BUCK3
6) For further investigation we disconnected GPIO8, GPIO10 and put there two pull ups instead. Then the retry behaviour is no longer visible and the rails come up without retring and also the POR reset signals from PMIC to SOC (NRESETOUT and GPIO11) are released.
Unfortunatelly trough the high on GPIO8 during power up the BUCK5 is obviously not switched on and therefore also not LDO_C (missing enable from VDD_MCU_0V85).
What could be the root cause for the
a) high current flow there on BUCK3 (we did an x-ray of the board so there should be no soldering issues)
b) why the problem with BUCK3 obviously does not exist with the option described under 6)
What else can we check or which other signals can may influence the power up of the PMIC?
Thanks for you answer in advance.
Kind regards
Thomas Paula
PMIC register dump from address 0x48. (offset in decimal)
[0] '\0' (0x00)
[1] '‚' (0x82)
[2] ':' (0x3A)
[3] '.' (0x03)
[4] '"' (0x22)
[5] ',' (0x2C)
[6] '"' (0x22)
[7] ',' (0x2C)
[8] '"' (0x22)
[9] ',' (0x2C)
[10] '"' (0x22)
[11] '+' (0x2B)
[12] '"' (0x22)
[13] '.' (0x1C)
[14] 's' (0x73)
[15] 's' (0x73)
[16] 's' (0x73)
[17] 's' (0x73)
[18] 'A' (0x41)
[19] 'A' (0x41)
[20] '²' (0xB2)
[21] '²' (0xB2)
[22] 'A' (0x41)
[23] 'A' (0x41)
[24] '.' (0x1B)
[25] '.' (0x1B)
[26] '.' (0x1B)
[27] '.' (0x1B)
[28] '.' (0x1B)
[29] ' ' (0x20)
[30] ' ' (0x20)
[31] ' ' (0x20)
[32] ' ' (0x20)
[33] '\0' (0x00)
[34] '\0' (0x00)
[35] '8' (0x38)
[36] 'ô' (0xF4)
[37] '.' (0x10)
[38] '8' (0x38)
[39] '.' (0x1B)
[40] '.' (0x1B)
[41] '.' (0x1B)
[42] '.' (0x1B)
[43] '.' (0x01)
[44] '?' (0x3F)
[45] '\0' (0x00)
[46] '\0' (0x00)
[47] '\0' (0x00)
[48] '\0' (0x00)
[49] ' ' (0x20)
[50] '@' (0x40)
[51] 'P' (0x50)
[52] 'Ð' (0xD0)
[53] '.' (0x01)
[54] '.' (0x03)
[55] '0' (0x30)
[56] '.' (0x18)
[57] '.' (0x01)
[58] '.' (0x10)
[59] 'C' (0x43)
[60] '.' (0x01)
[61] '\0' (0x00)
[62] '\0' (0x00)
[63] '\0' (0x00)
[64] '\b' (0x08)
[65] '¥' (0xA5)
[66] '•' (0x95)
[67] '.' (0x05)
[68] '.' (0x1E)
[69] '.' (0x01)
[70] 'U' (0x55)
[71] 'Õ' (0xD5)
[72] '.' (0x1D)
[73] '.' (0x03)
[74] '3' (0x33)
[75] '.' (0x03)
[76] '3' (0x33)
[77] '3' (0x33)
[78] '\0' (0x00)
[79] 'ÿ' (0xFF)
[80] 'ÿ' (0xFF)
[81] '?' (0x3F)
[82] '.' (0x11)
[83] '.' (0x02)
[84] '0' (0x30)
[85] '\0' (0x00)
[86] '\0' (0x00)
[87] '\0' (0x00)
[88] '\0' (0x00)
[89] '\0' (0x00)
[90] '»' (0xBB)
[91] '.' (0x06)
[92] '\0' (0x00)
[93] '\b' (0x08)
[94] '.' (0x02)
[95] '.' (0x02)
[96] '\0' (0x00)
[97] '@' (0x40)
[98] '\0' (0x00)
[99] '\0' (0x00)
[100] '\0' (0x00)
[101] '.' (0x02)
[102] '.' (0x01)
[103] '\n' (0x0A)
[104] '\0' (0x00)
[105] '.' (0x06)
[106] '\0' (0x00)
[107] '\0' (0x00)
[108] '\0' (0x00)
[109] '\0' (0x00)
[110] '\0' (0x00)
[111] '\0' (0x00)
[112] '\0' (0x00)
[113] '\0' (0x00)
[114] '\0' (0x00)
[115] '.' (0x02)
[116] '\0' (0x00)
[117] '\0' (0x00)
[118] '\0' (0x00)
[119] '\0' (0x00)
[120] '\0' (0x00)
[121] '\0' (0x00)
[122] '\0' (0x00)
[123] '\0' (0x00)
[124] '\0' (0x00)
[125] '\0' (0x00)
[126] '\0' (0x00)
[127] '\0' (0x00)
[128] '\0' (0x00)
[129] '\f' (0x0C)
[130] '.' (0x18)
[131] '.' (0x0F)
[132] '.' (0x0F)
[133] '\0' (0x00)
[134] '\0' (0x00)
[135] '.' (0x1F)
[136] '\0' (0x00)
[137] '\0' (0x00)
[138] '.' (0x1F)
[139] '\v' (0x0B)
[140] 'ÿ' (0xFF)
[141] 'ÿ' (0xFF)
[142] '\0' (0x00)
[143] '\0' (0x00)
[144] '\0' (0x00)
[145] '\0' (0x00)
[146] '\0' (0x00)
[147] '\0' (0x00)
[148] '\0' (0x00)
[149] '\0' (0x00)
[150] '\0' (0x00)
[151] '\0' (0x00)
[152] '\0' (0x00)
[153] '\0' (0x00)
[154] '\0' (0x00)
[155] '\0' (0x00)
[156] '\0' (0x00)
[157] '\0' (0x00)
[158] '\0' (0x00)
[159] '\0' (0x00)
[160] '\0' (0x00)
[161] '\0' (0x00)
[162] '\0' (0x00)
[163] '€' (0x80)
[164] '\0' (0x00)
[165] '\0' (0x00)
[166] '\b' (0x08)
[167] '\0' (0x00)
[168] '\0' (0x00)
[169] '\0' (0x00)
[170] '\0' (0x00)
[171] '\0' (0x00)
[172] '\0' (0x00)
[173] '\0' (0x00)
[174] '\0' (0x00)
[175] '\0' (0x00)
[176] '\0' (0x00)
[177] '\0' (0x00)
[178] '\0' (0x00)
[179] '\0' (0x00)
[180] '\0' (0x00)
[181] '\0' (0x00)
[182] '\0' (0x00)
[183] '\0' (0x00)
[184] '.' (0x01)
[185] '.' (0x01)
[186] '\0' (0x00)
[187] '\0' (0x00)
[188] '\0' (0x00)
[189] '\0' (0x00)
[190] '\0' (0x00)
[191] '\0' (0x00)
[192] '\0' (0x00)
[193] '\0' (0x00)
[194] '\0' (0x00)
[195] 'à' (0xE0)
[196] '€' (0x80)
[197] '\0' (0x00)
[198] '\0' (0x00)
[199] '\0' (0x00)
[200] '\0' (0x00)
[201] '\0' (0x00)
[202] '\0' (0x00)
[203] '\0' (0x00)
[204] '.' (0x01)
[205] '-' (0x2D)
[206] '' (0x9D)
[207] '\0' (0x00)
[208] '\0' (0x00)
[209] '\0' (0x00)
[210] '\0' (0x00)
[211] '\0' (0x00)
[212] '\0' (0x00)
[213] '\0' (0x00)
[214] '\0' (0x00)
[215] '\0' (0x00)
[216] '\0' (0x00)
[217] '\0' (0x00)
[218] '\0' (0x00)
[219] '\0' (0x00)
[220] '\0' (0x00)
[221] '\0' (0x00)
[222] '\0' (0x00)
[223] '\0' (0x00)
[224] '\0' (0x00)
[225] '\0' (0x00)
[226] '\0' (0x00)
[227] '\0' (0x00)
[228] '\0' (0x00)
[229] '\0' (0x00)
[230] '\0' (0x00)
[231] '\0' (0x00)
[232] '\0' (0x00)
[233] '\0' (0x00)
[234] '\0' (0x00)
[235] '\0' (0x00)
[236] '\0' (0x00)
[237] '\0' (0x00)
[238] '\0' (0x00)
[239] '\0' (0x00)
[240] '\0' (0x00)
[241] '\0' (0x00)
[242] '\0' (0x00)
[243] '\0' (0x00)
[244] '\0' (0x00)
[245] '\0' (0x00)
[246] '\0' (0x00)
[247] '\0' (0x00)
[248] '\0' (0x00)
[249] '\0' (0x00)
[250] '\0' (0x00)
[251] '\0' (0x00)
[252] '\0' (0x00)
[253] '\0' (0x00)
[254] '\0' (0x00)
[255] '\0' (0x00)