Part Number: PROCESSOR-SDK-J721E
we are trying to connect to a Slave device (Power over coax) over I2C0. we have initiated read request to the slave through the TI I2C driver API I2C_transfer (). we have observed that communication sequence has started with 7-bit slave address(0x28) being sent on the I2C0 bus and we have also received ACK for the address data, but as soon as the ACK for slave address byte is received, we could see that I2C SCL line pulled low and the communication with the slave device is stopped. Please refer to the attachment from CRO probe on I2C0 bus.
Can you please guide us to debug this issue of SCL line continuously pulled Low.