Other Parts Discussed in Thread: BIOSLINUXMCSDK
Hi.
My develoment platform is below.
DSP: C6474 1GHz
DDR2: 512MB
BIOS: 5.4
NDK: 2.0
CSL: 3.0.3
CCS: 3.3
When I transfer NDK data to DDR2 with writen below command I've got problem network stack is not working.
============================================================================================================
SECTIONS
{
.far:NDK_PACKETMEM {} align=128 > DDR2
.far:NDK_MMBUFFER {} align=128 >DDR2
.far:NDK_OBJMEM {} align=128 > DDR2
}
============================================================================================================
Is there any software version conflict in my development environment, or any other problem for this command.
Additionally, after boot NDK, first ping is working, but after stay for several time when I send ping, dosen't response. Is there anyone have same problem ?