This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Can I use two timers on DSP1?

Part Number: AM5728
Other Parts Discussed in Thread: SYSBIOS

My application need to use timer5 and timerX on DSP1, which use timer6 on DSP2, and I would prefer to disable IPU1&2, but question is how to assign the timer11 to DSP1 on linux DTS side?

Thanks!

&ipu1 {
status = "disable";
//timers = <&timer11>;
//watchdog-timers = <&timer7>, <&timer8>;
timers = <>;
watchdog-timers = <>;
};

&ipu2 {
status = "disable";
timers = <>;//<&timer3>;
watchdog-timers = <>;//<&timer12>, <&timer9>;
};

&dsp1 {
status = "okay";
memory-region = <&dsp1_cma_pool>;
mboxes = <&mailbox5 &mbox_dsp1_ipc3x>;
//timers = <&timer5>;
//timers = <&timer5>, <&timer6>;
timers = <&timer5>, <&timer11>;
//timers = <&timer5>, <&timer9>;
watchdog-timers = <&timer10>;
};

&dsp2 {
status = "okay";
memory-region = <&dsp2_cma_pool>;
mboxes = <&mailbox6 &mbox_dsp2_ipc3x>;
timers = <&timer6>;
//timers = <&timer12>, <&timer9>;
watchdog-timers = <&timer13>;
};