Part Number: AM68A
Other Parts Discussed in Thread: , AM68
Hello Support Team,
Below are few queries that I need to be clear before procuring the AM68A processor and its EVK:
- Power consumption of the processor while encoding 4k60p data?
- As per the datasheet, AM68A9 supports MIPI-DPHY 1.2 and as per the standard, the speed should be 2.5Gbps per lane. But then in the datasheet, the speed mentioned is 1.5Gbps per lane. Could you confirm the supported speed for the same?
- Supported 4k60p CMOS module which is directly compatible with the evaluation kit.
- Please share the processor's encoder latency data.
Regards,
Bino Mani