Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: AM6442, SYSCONFIG
Given what Kai on CCS support has stated about taking a previous design example to modify the SysConfig file (in CCS v13) , I would like to see one of the following examples that involves an A53 on the AM6442 (any one would be sufficient):
1) A procedure to modify /add the A53 Linux core into a SysConfig tool generated design example that was taken from the MCU+ SDK (that uses only R5/M4 cores in FreeRTOS) to create a system design OR
2) A system design example (having a SysConfig tool generated file) that uses at least one A53 core in Linux and at least one R5 core in FreeRTOS , which then can be modified and/or expanded.
thanks
Jim Mrowca