Hi,
My system configuration consists of the following:
DM6467 729 MHz, 128 MB DDR2 400 MHz
TVP5158 configured to send 1 D1 (Non-interleaved, 27M,BT.656 mode) to DM6467.
My issue is that I get occasional errors in my acquired frames which I have debugged with the occurrence of VP_ERRINT (VPIF error interrupt that I have enabled). Those errors result in false color in some of my video frames . From the documentation (spruer9d), it says in 2.8.1 that such an error can either be due to:
- Internal buffer overflow
- Length of eav2sav or sav2eav is not the same as the configured value
- Bit error detected on 4th field of TRC