This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM69: WKUP_OSC0 changed - possible drawbacks

Part Number: AM69

Hello TI,

in our design, we want to use a 24 MHz clock as WKUP_OSC0 (main clock) instead of the 19.2 MHz used on the AM69-SK.

We set BOOTMODE MCU 0-2 pins accordingly (010, instead of 000).

Is there something else we should take into account?

The SW running on that board will be U-Boot / Linux (based on TI SDK).

I saw that in the device tree, there is a clk_19_2mhz: dummy_clock_19_2mhz that is not referenced anywhere.

Is there just for reference? From what I saw it is not referenced anywhere.

Thanks,

Kind regards.