This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 Byte Lanes

Can I route a board with the byte lanes between the DDR3 UDIMM and C667x reversed? 

0->7

1->6

2->5

3->4

...

instead of

0->0

1->1

2->2

3->3

...

Or will this wreak havoc with the write and read leveling due to some timing dependence in the DSP memory controller? Looking at the specs for the DIMM and individual DDR3 ICs, there should not be a problem on that end. 

Thanks,

Colin

  • Each byte lane should converge independently during leveling so it shouldn't make any difference if you switch the order.  Make sure that all of the associated signals for each byte lane (Data, DQSp/n, DQM)  are swapped and that all the length matching requirements for these signals are met.  As long as you calculate the proper lengths for the address and command signals when calculating the registers settings you shouldn't have a problem.