Hi
May I have question about external serdes refclk?
My customer is using AM6442 and serdes use for PCIe.
Q1
I think EVM is using HCSL 100MHz clock.

Can only input HCSL level clock generator?
Q2 :
In TRM, looks Serdes can use internal clock.
If use this internal clock, Is external clock input not need?

Q3 :
I think Serdes supporting 19.2, 20, 24, 25, 26, 27, 100MHz clock frequency.
Is this mean Refclk input frequency?

Or Refclk input is 100MHz or 125MHz only, and internally generate 19.2, 20, 24, 25, 26, 27,100 MHz?

Thanks,
GR