This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can I use the XDS100V2 emulator to bring up DDR3 on my custom DM8168 board?



Hi, all

We have developped our custom DM8168 board which using DDR3 memory. And as SPRABJ3 metioned, It should Calculate the static values using CCS and XDS560 emulator.

Because XDS100V2 is  cheaper than XDS560. I wonder if XDS100V2 emulator can be used instead of  XDS560 for DM8168?

And what is the different between XDS100V2 and XDS560 beside of the speed.

 

Thank you!

Matt