Other Parts Discussed in Thread: TMS320C6678
Hi All ,
I have been testing the PCIe boot sample application present in MCSDK 2.0.0.11(..tools/bootloader/examples/pcie). My test setup includes Linux PC and TMS320C6678 EVM. I was able to boot the hello world sample application from Shannon via PCIe link between the linux PC and the EVM.
I would now like to boot my custom SYS-BIOS application via PCIe. To test this i used the led play application mentioned in MCSDK user guide document (http://processors.wiki.ti.com/index.php?title=BIOS_MCSDK_2.0_User_Guide#Example_2_-_Building_and_running_your_first_tasking_application_using_MCSDK_and_BIOS). This application runs a background tak that will flash an on board LED. I followed the steps mentioned below to test the applciation to boot via PCIe.
1) Built the led_play application to generate the .out file
2) Converted the out file to .h file by executing helloworld_elf2HBin.bat . I had renamed the led_play.out file to pcieboot_helloworld_evm6678l.out to be able to be picked up by helloworld_elf2HBin.bat tool.
3) I than generated the .ko file on my linux PC using this .h file.
4) When insmod the .ko file i observe the following output message from the main function of LED play applciation
Start BIOS 6
5) The LEDs on the board do not toggle and there are no output messages from the ledPlayTask function
6)I am not sure why the task is not being executed and LEDS are not being toggled. The Start BIOS 6 output message indicates that the control is being transferred to the application. However the task seems to have not been launched.I have tested the led_play application to boot properly from NOR flash .
Can anyone advice if i have missed out any steps .Is my assumption that the PCIe boot sample application (present in MCSDK release )can be used to boot any custom application via PCIe wrong? Is there any other dependencies that i have missed ?
-Anil