This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: LSC Tuning output

Part Number: SK-AM62A-LP

Hello Ti,

Currently I am working on LSC(Lens Shading Correction) for IMX219

1. As the code mentioned in this link we have generated LUT file but how to use that text file for LSC tuning

/cfs-file/__key/communityserver-discussions-components-files/791/J7_5F00_ISP_5F00_LSC.pdf


2. For IMX219 we have this spec_file

Image Height Relative Illmination
mm
0.00 100%
0.11 99.98%
0.23 99.91%
0.34 99.80%
0.46 99.65%
0.57 98.74%
0.69 98.38%
0.80 96.94%
0.92 93.90%
1.03 92.09%
1.15 89.83%
1.26 86.69%
1.38 84.52%
1.49 81.87%
1.61 78.31%
1.72 75.15%
1.84 70.52%
1.95 66.71%
2.07 60.96%
2.18 56.19%
2.30 47.33%



so after adding this spec_file we are not getting proper tunning graph

3. How to Interleave 2D gain map arrays for different color channels??

4. If we use Matlab code then how to use that generated LUT file in .xml 

  • Hi Atharva,

    so after adding this spec_file we are not getting proper tunning graph

    Yes, that plot shows that tuning is not done properly.

    Did you follow the plugin guide to input all the required information correctly?

    2. For IMX219 we have this spec_file

    This is good for lens spec.

    Did you follow the plugin guide and convert it to the proper format?

  • Hi Gang Hua,

    What is the proper format of that spec file

  • What is the proper format of that spec file

    Hi Atharva,

    Please take a look at the LSC plugin guide under the help menu of tuning tool.
    The input LUT for tuning tool has the 1st column in the unit of pixels.

  • Hello Gang Hua,

    Just tell me if I want to remove Greenish at center through LSC then what shape graph should i get so that i can work accordingly.

    Or if you have any reference graph for same then it will be helpful.

    This is my current Graph:




    This is the LUT file which we are currently using in which left column is number of pixels and second column is relative Illumination:

    0   1
    49   0.9998
    103   0.9991
    152   0.998
    205   0.9965
    254   0.9874
    308   0.9838
    357   0.9694
    411   0.939
    460   0.9209
    513   0.8983
    563   0.8669
    616   0.8452
    665   0.8187
    718   0.7831
    768   0.7515
    821   0.7052
    871   0.6671
    924   0.6096
    973   0.5619
    1027   0.4733

    Thanks

  • This is the LUT file which we are currently using in which left column is number of pixels and second column is relative Illumination:

    Simple LSC LUT like this is for making the image corner as bright as image center (i.e., undo lens shading).
    That won't change any color.

    Just tell me if I want to remove Greenish at center through LSC then what shape graph should i get so that i can work accordingly.

    Color shading may be handled by applying different LSC gains on the R/G/B channels.
    As the shape of these R/G/B LUTs are different, it can change the color of things.
    You will have to calibrate your lens and find out different LUTs for R/G/B pixels.

    Tuning tool does not support this directly if I remember correctly.
    You may have to use the tuning tool to generate xml files from R/G/B input LUTs and manually interleave the gains for the final xml file.

  • Simple LSC LUT like this is for making the image corner as bright as image center (i.e., undo lens shading).
    That won't change any color.

    Then which LUT will remove the greenish colour at the center

  • Then which LUT will remove the greenish colour at the center

    It is the combination of all R/G/B LUTs.

    For example, around the image center, we would expect to have R and B gains higher than G gains in your case.

    That shall change the greenish tone around image center.
    However, as the amount of color shading may change according to the type of lighting you have, you may have to adapt LSC tuning to lighting conditions.
    If you don't have much experience or the necessary H/W equipment for ISP tuning, it is much easier to use a better camera-lens module.

  • You will have to calibrate your lens and find out different LUTs for R/G/B pixels.

    Can you tell me how I can take different raw images with R/G/B 

  • Can you tell me how I can take different raw images with R/G/B 

    I am not sure if I understand you correctly.

    Raw image is the same, but LSC LUTs are different.
    The raw sensor image is in Bayer RGGB pattern.