Hi,
I am using the C5515 EVM with the ECG MDK daughter card. I cannot get the SD/MMC CSL examples to work when the MDK daughter card is connected to the EVM. They work perfectly fine when the daughter card is not connected. I saw an earlier post http://e2e.ti.com/support/dsp/tms320c5000_power-efficient_dsps/f/109/p/43285/169819.aspx#169819 with the same issue; but there was no answer posted in that thread. Is there a software setting or a hardware limitation that is causing this issue? Thank you for any help with this.