Other Parts Discussed in Thread: AM3505
DEar Sir,
I have a design which using AM3505, I expected USB OTG port can automatically config to a host or a device, but now , we found it is not able to change the config after system boot up. The case is once I config the OTG to Host port then it is a host even I re-config to slave, it still be a host. if I config it to slave and then re-boot system then the OTG will become slave port. any ideal?
Note: I my design the USB OTG pin 5 "ID pin" is connected to external USB device
BR
Edwin