This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CMEMK configurations on loadmodule-rc



I had posted this before, but I still trying to debug this problem, about seeting the configurations of the CMEMK on the loadmodule-rc

this is the original configurations of the CMEMK on the loadmodule-rc file

load () {
    modprobe cmemk phys_start=0x83C00000 phys_end=0x88000000 allowOverlap=1 phys_start_1=0x00001000 phys_end_1=0x00008000 pools_1=1x28672 useHeapIfPoolUnavailable=1


but I want this configuration of the cmemk to be like this

cmemk phys_start=0x84c00000 phys_end=0x88000000 pools=8x46672

so I made this changes on the load module

load () {
    modprobe cmemk phys_start=0x84c00000 phys_end=0x88000000 pools=8x46672 allowOverlap=1 phys_start_1=0x00001000 phys_end_1=0x00008000 pools_1=1x28672 useHeapIfPoolUnavailable=1

but it does not seem to work, because if it did capture_prev_rsz_onthe_fly_bayer_mew  would had work, because when I do rmmod cmemk and then insmod cmemk with this configurations

cmemk phys_start=0x84c00000 phys_end=0x88000000 pools=8x46672

the program works, so how can I made this configuration to load automaticly on the loadmodule-rc

root@dm368-evm:/usr/share/ti/linux-driver-examples/imp-prev-rsz# ./capture_prev_
rsz_onthe_fly_bayer_mew -i1 -m4 -h60                                           
input_std_paramsCMEMK Error: ALLOC: invalid pool (0) passed.                   
: name = V4L2_STD_720P_30                                                      
input_std_params: output size = 1280 * 720                                     
calling cmem utilities for allocating frame buffers                            
CMEM Error: allocPool: ioctl CMEM_IOCALLOC failed from pool 0: -1              
Failed to allocate cmem pool                                                   
Unable to Allocate user buffers 

 

Regards,

Andre