Hello,
I have updated the SDK from using 09_00_00_07 to now using 09_02_00_05.
After updating I am having trouble building tisdk-default-image, and specifically the gn-native_111.0.5563.64.bb recipe.
Here is the build log:
DEBUG: Executing shell function do_compile
ninja: Entering directory `/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/chromium-111.0.5563.64/out/Release/gn_build'
[1/195] CXX src/base/files/file_path_constants.o
FAILED: src/base/files/file_path_constants.o
clang++ -target x86_64-linux -MMD -MF src/base/files/file_path_constants.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/files/file_path_constants.cc -o src/base/files/file_path_constants.o
../../../tools/gn/src/base/files/file_path_constants.cc:7:10: fatal error: 'iterator' file not found
#include <iterator>
^~~~~~~~~~
1 error generated.
[2/195] CXX src/base/files/scoped_file.o
FAILED: src/base/files/scoped_file.o
clang++ -target x86_64-linux -MMD -MF src/base/files/scoped_file.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/files/scoped_file.cc -o src/base/files/scoped_file.o
In file included from ../../../tools/gn/src/base/files/scoped_file.cc:5:
../../../tools/gn/src/base/files/scoped_file.h:10:10: fatal error: 'memory' file not found
#include <memory>
^~~~~~~~
1 error generated.
[3/195] CXX src/base/command_line.o
FAILED: src/base/command_line.o
clang++ -target x86_64-linux -MMD -MF src/base/command_line.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/command_line.cc -o src/base/command_line.o
In file included from ../../../tools/gn/src/base/command_line.cc:5:
../../../tools/gn/src/base/command_line.h:19:10: fatal error: 'map' file not found
#include <map>
^~~~~
1 error generated.
[4/195] CXX src/base/files/file_path.o
FAILED: src/base/files/file_path.o
clang++ -target x86_64-linux -MMD -MF src/base/files/file_path.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/files/file_path.cc -o src/base/files/file_path.o
In file included from ../../../tools/gn/src/base/files/file_path.cc:5:
../../../tools/gn/src/base/files/file_path.h:107:10: fatal error: 'iosfwd' file not found
#include <iosfwd>
^~~~~~~~
1 error generated.
[5/195] CXX src/base/files/scoped_temp_dir.o
FAILED: src/base/files/scoped_temp_dir.o
clang++ -target x86_64-linux -MMD -MF src/base/files/scoped_temp_dir.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/files/scoped_temp_dir.cc -o src/base/files/scoped_temp_dir.o
In file included from ../../../tools/gn/src/base/files/scoped_temp_dir.cc:5:
In file included from ../../../tools/gn/src/base/files/scoped_temp_dir.h:20:
../../../tools/gn/src/base/files/file_path.h:107:10: fatal error: 'iosfwd' file not found
#include <iosfwd>
^~~~~~~~
1 error generated.
[6/195] CXX src/base/environment.o
FAILED: src/base/environment.o
clang++ -target x86_64-linux -MMD -MF src/base/environment.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/environment.cc -o src/base/environment.o
In file included from ../../../tools/gn/src/base/environment.cc:5:
../../../tools/gn/src/base/environment.h:8:10: fatal error: 'map' file not found
#include <map>
^~~~~
1 error generated.
[7/195] CXX src/base/files/file.o
FAILED: src/base/files/file.o
clang++ -target x86_64-linux -MMD -MF src/base/files/file.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/files/file.cc -o src/base/files/file.o
In file included from ../../../tools/gn/src/base/files/file.cc:5:
../../../tools/gn/src/base/files/file.h:10:10: fatal error: 'string' file not found
#include <string>
^~~~~~~~
1 error generated.
[8/195] CXX src/base/files/file_enumerator.o
FAILED: src/base/files/file_enumerator.o
clang++ -target x86_64-linux -MMD -MF src/base/files/file_enumerator.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/files/file_enumerator.cc -o src/base/files/file_enumerator.o
In file included from ../../../tools/gn/src/base/files/file_enumerator.cc:5:
../../../tools/gn/src/base/files/file_enumerator.h:11:10: fatal error: 'vector' file not found
#include <vector>
^~~~~~~~
1 error generated.
[9/195] CXX src/base/json/json_parser.o
FAILED: src/base/json/json_parser.o
clang++ -target x86_64-linux -MMD -MF src/base/json/json_parser.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/json/json_parser.cc -o src/base/json/json_parser.o
In file included from ../../../tools/gn/src/base/json/json_parser.cc:5:
../../../tools/gn/src/base/json/json_parser.h:11:10: fatal error: 'memory' file not found
#include <memory>
^~~~~~~~
1 error generated.
[10/195] CXX src/base/files/file_util.o
FAILED: src/base/files/file_util.o
clang++ -target x86_64-linux -MMD -MF src/base/files/file_util.o.d -I../../../tools/gn/src -I. -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -isystem/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/include -O2 -pipe -D_LIBCPP_HAS_NO_VENDOR_AVAILABILITY_ANNOTATIONS -DNDEBUG -O3 -fdata-sections -ffunction-sections -Werror -D_FILE_OFFSET_BITS=64 -D__STDC_CONSTANT_MACROS -D__STDC_FORMAT_MACROS -pthread -pipe -fno-exceptions -fno-rtti -fdiagnostics-color -Wall -Wextra -Wno-unused-parameter -Wextra-semi -Wundef -std=c++17 -c ../../../tools/gn/src/base/files/file_util.cc -o src/base/files/file_util.o
In file included from ../../../tools/gn/src/base/files/file_util.cc:5:
../../../tools/gn/src/base/files/file_util.h:15:10: fatal error: 'set' file not found
#include <set>
^~~~~
1 error generated.
ninja: build stopped: subcommand failed.
Traceback (most recent call last):
File "/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/chromium-111.0.5563.64/tools/gn/bootstrap/bootstrap.py", line 144, in <module>
sys.exit(main(sys.argv[1:]))
File "/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/chromium-111.0.5563.64/tools/gn/bootstrap/bootstrap.py", line 130, in main
subprocess.check_call(cmd)
File "/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/recipe-sysroot-native/usr/lib/python3.10/subprocess.py", line 369, in check_call
raise CalledProcessError(retcode, cmd)
subprocess.CalledProcessError: Command '['ninja', '-C', '/mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/chromium-111.0.5563.64/out/Release/gn_build', '-w', 'dupbuild=err', 'gn']' returned non-zero exit status 1.
WARNING: /mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/temp/run.do_compile.1266257:149 exit 1 from 'python3 /mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/chromium-111.0.5563.64/tools/gn/bootstrap/bootstrap.py --skip-generate-buildfiles'
WARNING: Backtrace (BB generated script):
#1: do_compile, /mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/temp/run.do_compile.1266257, line 149
#2: main, /mnt/datassd/ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03/yocto-build/build/arago-tmp-default-glibc/work/x86_64-linux/gn-native/111.0.5563.64-r0/temp/run.do_compile.1266257, line 153
I would be very thankful for any help in resolving this.
Regards,
Mattias