Other Parts Discussed in Thread: SYSBIOS, TMS320DM6446
Hi,
I am using CCS V5.1 with a custom DM6446 board. I am trying to run some of the example programs that came with CCS V5.1, such as "task mutex" and "static" examples. The compile was OK with both examples but the program did not give any results (SYSTEM_printf() does not work) when running. It seems that the program got stuck after the BIOS_start() function call and the tasks (either dynamically created or statically created) were not running. The top part of the map file is as follows. Any help or pointers would be greatly appreciated.
Zhao
******************************************************************************
TMS320C6x Linker PC v7.2.1
******************************************************************************
>> Linked Fri Sep 23 17:05:03 2011
OUTPUT FILE NAME: <sysbios_task_example.out>
ENTRY POINT SYMBOL: "_c_int00" address: 87605160
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
ARM_RAM 10008000 00004000 00002000 00002000 RW
IRAM 11800000 00008000 00000000 00008000 RW X
L1DSRAM 11f04000 0000c000 00000000 0000c000 RW
DDR 87600000 00800000 0000db90 007f2470 RW X
DSPLINKMEM 87e00000 00100000 00000000 00100000 RW X
RESET_VECTOR 87f00000 00000080 00000000 00000080 RW X