Part Number: AM62A7-Q1
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
We are working on a memtester on a custom board with 4GB DDR.
When running memtester, an error and kernel panic occur as shown below.
Is there any point for debugging?
log_1:
root@am62axx-evm:~# memtester 3100M memtester version 4.5.1 (64-bit) Copyright (C) 2001-2020 Charles Cazabon. Licensed under the GNU General Public License version 2 (only). pagesize is 4096 pagesizemask is 0xfffffffffffff000 want 3100MB (3250585600 bytes) got 3100MB (3250585600 bytes), trying mlock ...locked. Loop 1: Stuck Address : ok Random Value : ok Compare XOR : ok Compare SUB : ok Compare MUL : ok Compare DIV : ok Compare OR : ok Compare AND : ok Sequential Increment: ok Solid Bits : testing 0FAILURE: 0x00004000 != 0x00000000 at offset 0x00417b98. FAILURE: 0x00004000 != 0x00000000 at offset 0x01f342d8. FAILURE: 0x00004000 != 0x00000000 at offset 0x020532d8. FAILURE: 0x00004000 != 0x00000000 at offset 0x020e22d8. FAILURE: 0x00000000 != 0x00004000 at offset 0x021a8db8. FAILURE: 0x00004000 != 0x00000000 at offset 0x02287b88. FAILURE: 0x00004000 != 0x00000000 at offset 0x0b927dd8. FAILURE: 0x00004000 != 0x00000000 at offset 0x110d7918. FAILURE: 0x00004000 != 0x00000000 at offset 0x115b7df8. FAILURE: 0x00004000 != 0x00000000 at offset 0x1ad902d8. FAILURE: 0x00004000 != 0x00000000 at offset 0x1db97df8. FAILURE: 0x00000000 != 0x00004000 at offset 0x2d2b8df8. FAILURE: 0x00004000 != 0x00000000 at offset 0x30e27b88. FAILURE: 0x00000000 != 0x00004000 at offset 0x36278db8. FAILURE: 0x00004000 != 0x00000000 at offset 0x36467df8. FAILURE: 0x00004000 != 0x00000000 at offset 0x36a57df8. FAILURE: 0x00004000 != 0x00000000 at offset 0x3a1c06e8. FAILURE: 0x00000000 != 0x00004000 at offset 0x3f797c28. FAILURE: 0x00004000 != 0x00000000 at offset 0x42117b18. FAILURE: 0x00004000 != 0x00000000 at offset 0x42627bc8. FAILURE: 0x00004000 != 0x00000000 at offset 0x42c97808. FAILURE: 0x00000000 != 0x00004000 at offset 0x42e48df8. FAILURE: 0x00004000 != 0x00000000 at offset 0x430e7bd8. FAILURE: 0x00004000 != 0x00000000 at offset 0x432502d8. FAILURE: 0x00004000 != 0x00000000 at offset 0x44977df8. FAILURE: 0x00004000 != 0x00000000 at offset 0x45d57df8. FAILURE: 0x00004000 != 0x00000000 at offset 0x49776df8. FAILURE: 0x00004000 != 0x00000000 at offset 0x519942e8. FAILURE: 0x00004000 != 0x00000000 at offset 0x5e8c02d8. Block Sequential : testing 36[ 302.245275] Unable to handle kernel NULL pointer dereference at virtual address 00000000000000c0 [ 302.254071] Mem abort info: [ 302.256861] ESR = 0x0000000096000006 [ 302.260602] EC = 0x25: DABT (current EL), IL = 32 bits [ 302.265907] SET = 0, FnV = 0 [ 302.268953] EA = 0, S1PTW = 0 [ 302.272086] FSC = 0x06: level 2 translation fault [ 302.276955] Data abort info: [ 302.279829] ISV = 0, ISS = 0x00000006 [ 302.283655] CM = 0, WnR = 0 [ 302.286615] user pgtable: 4k pages, 48-bit VAs, pgdp=000000088593e000 [ 302.293044] [00000000000000c0] pgd=08000008859ac003, p4d=08000008859ac003, pud=08000008859ab003, pmd=0000000000000000 [ 302.303649] Internal error: Oops: 0000000096000006 [#1] PREEMPT SMP [ 302.309907] Modules linked in: ipv6 [ 302.313398] CPU: 3 PID: 0 Comm: swapper/3 Not tainted 6.1.46-g247b2535b2 #1 [ 302.320349] Hardware name: Texas Instruments AM62A7 SK (DT) [ 302.325911] pstate: 600000c5 (nZCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 302.332862] pc : unregister_fair_sched_group+0x74/0x180 setting 37[ 302.338091] lr : check_preempt_curr+0x4c/0x8c [ 302.344346] sp : ffff8000093e3e80 [ 302.347648] x29: ffff8000093e3e80 x28: ffff0008001b0e40 x27: 0000000000000000 [ 302.354784] x26: ffff0008001b0e40 x25: 0000000000000000 x24: 0000000000000000 [ 302.361909] x23: 0000000000000000 x22: 00000000000000c0 x21: 0000000000000020 [ 302.369034] x20: ffff000800efe3c0 x19: 0000000000000003 x18: 0000000000000000 [ 302.376158] x17: ffff8008767ae000 x16: ffff8000093e0000 x15: 0000000000000400 [ 302.383284] x14: 00000000000000be x13: 0000000000000000 x12: 0000000000000000 [ 302.390408] x11: 0000000000000040 x10: 00000000000000db x9 : 0000000000000000 [ 302.397535] x8 : ffff8008767ae000 x7 : 0000000000000003 x6 : 0000000000000007 [ 302.404659] x5 : ffff800008f94e40 x4 : ffff800008f94d70 x3 : ffff8008767ae000 [ 302.411783] x2 : ffff0008001b0e40 x1 : 0000000000000003 x0 : 0000000000000003 [ 302.418915] Call trace: [ 302.421353] unregister_fair_sched_group+0x74/0x180 [ 302.426223] check_preempt_curr+0x4c/0x8c [ 302.430227] ttwu_do_wakeup.constprop.0+0x1c/0xa4 [ 302.434926] ttwu_do_activate.isra.0+0xb4/0xec [ 302.439361] sched_ttwu_pending+0xa8/0x144 [ 302.443451] __flush_smp_call_function_queue+0xdc/0x254 [ 302.448670] generic_smp_call_function_single_interrupt+0x14/0x20 [ 302.454753] ipi_handler+0xac/0x150 [ 302.458234] handle_percpu_devid_irq+0x84/0x130 [ 302.462762] generic_handle_domain_irq+0x2c/0x44 [ 302.467373] gic_handle_irq+0x50/0x124 [ 302.471124] call_on_irq_stack+0x24/0x4c [ 302.475041] do_interrupt_handler+0x80/0x8c [ 302.479217] el1_interrupt+0x34/0x70 [ 302.482792] el1h_64_irq_handler+0x18/0x2c [ 302.486878] el1h_64_irq+0x64/0x68 [ 302.490270] arch_cpu_idle+0x18/0x2c [ 302.493837] default_idle_call+0x30/0x6c [ 302.497755] do_idle+0x248/0x2c0 [ 302.500977] cpu_startup_entry+0x24/0x30 [ 302.504891] secondary_start_kernel+0x11c/0x140 [ 302.509412] __secondary_switched+0xb0/0xb4 [ 302.513599] Code: 91050318 9134e339 9410e5bd aa0003f3 (b94002c1) [ 302.519684] ---[ end trace 0000000000000000 ]--- [ 302.524293] Kernel panic - not syncing: Oops: Fatal exception in interrupt [ 302.531156] SMP: stopping secondary CPUs [ 302.535074] Kernel Offset: disabled [ 302.538550] CPU features: 0x00000,00800084,0000420b [ 302.543416] Memory Limit: none [ 302.546461] ---[ end Kernel panic - not syncing: Oops: Fatal exception in interrupt ]---
log_2:
root@am62axx-evm:~# memtester 3100M[ 12.454615] platform regulator-3: deferred probe pending memtester version 4.5.1 (64-bit) Copyright (C) 2001-2020 Charles Cazabon. Licensed under the GNU General Public License version 2 (only). pagesize is 4096 pagesizemask is 0xfffffffffffff000 want 3100MB (3250585600 bytes) got 3100MB (3250585600 bytes), trying mlock ...locked. Loop 1: Stuck Address : ok Random Value : ok Compare XOR : ok Compare SUB : ok Compare MUL : ok Compare DIV : ok Compare OR : ok Compare AND : ok Sequential Increment: ok Solid Bits : testing 49FAILURE: 0x00004000 != 0x00000000 at offset 0x0dd54d60. Block Sequential : testing 227[ 913.084087] Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP [ 913.092450] Modules linked in: ipv6 [ 913.095946] CPU: 1 PID: 1 Comm: systemd Not tainted 6.1.46-g247b2535b2 #1 [ 913.102726] Hardware name: Texas Instruments AM62A7 SK (DT) [ 913.108288] pstate: 20000005 (nzCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 913.115240] pc : link_path_walk.part.0.constprop.0+0x98/0x3d0 [ 913.120990] lr : path_openat+0xa4/0xe50 [ 913.124823] sp : ffff80000940bb20 [ 913.128131] x29: ffff80000940bb40 x28: ffff80000940bc50 x27: ffff000805941020 [ 913.135262] x26: 0000000000000000 x25: 0000000000000000 x24: 0000000000000001 [ 913.142391] x23: ffff80000940bc50 x22: ffff000800108000 x21: ffff000805941021 [ 913.149522] x20: ffff80000940bd74 x19: 0000000005941020 x18: 0000000000000000 [ 913.156652] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000 [ 913.163781] x14: 0000000000000000 x13: 0000000000000000 x12: 0000000000000000 [ 913.170911] x11: fefefefefefefeff x10: 0000fffffffffff8 x9 : 0000000000000000 [ 913.178041] x8 : ffff0008035af900 x7 : 0000000000000000 x6 : 000000000000003f [ 913.185171] x5 : 0000000000000013 x4 : ffff000800108000 x3 : 0000000000000000 [ 913.192301] x2 : 0000000000000000 x1 : ffff80000940bc50 x0 : 0000000000000070 [ 913.199432] Call trace: [ 913.201873] link_path_walk.part.0.constprop.0+0x98/0x3d0 [ 913.207270] path_openat+0xa4/0xe50 [ 913.210756] do_filp_open+0x84/0x134 [ 913.214331] do_sys_openat2+0xbc/0x174 [ 913.218077] __arm64_sys_openat+0x64/0xb0 [ 913.222082] invoke_syscall+0x48/0x114 [ 913.225831] el0_svc_common.constprop.0+0x44/0xfc [ 913.230533] do_el0_svc+0x20/0x30 [ 913.233847] el0_svc+0x28/0xa0 [ 913.236906] el0t_64_sync_handler+0xbc/0x140 [ 913.241173] el0t_64_sync+0x18c/0x190 [ 913.244839] Code: a94563f7 910203ff d50323bf d65f03c0 (d29a1a18) [ 913.250926] ---[ end trace 0000000000000000 ]--- [ 913.255640] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b [ 913.263296] SMP: stopping secondary CPUs [ 913.267221] Kernel Offset: disabled [ 913.270700] CPU features: 0x00000,00800084,0000420b [ 913.275569] Memory Limit: none [ 913.278617] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b ]---