Part Number: AM6442
Other Parts Discussed in Thread: IND-COMMS-SDK, SYSCONFIG, DP83869
Tool/software:
Hi,
I am working with the am64x on a phytec development board. I am trying to run the EtherCAT Example of the IND-COMMS-SDK (Version 09_01_00_03).
The default configuration of SysConfig for the PRU_IEP Signals does not work with the phytec board, since it uses the Pins for other purposes (for example PRG0_IEP0_EDC_SYNC_OUT1 Pin is used for INT/PWDN of the Ethernet PHY).
Now I am wondering if the signals for latch0/1 and sync0/1 are even required to be muxed onto a pin or whether it should work with configuring the time sync router of the am64x correctly and not mux the signals on the respective pins.
Kind regards,
Jakob