Hello everybody!
I would like to know whether there is a way to stream over ethernet without using the long caps config(string) described in the examples-wiki (http://processors.wiki.ti.com/index.php/Example_GStreamer_Pipelines#Network_Streaming).
I want to receive a stream from a VLC-Player with my DaVinci-Board, and therefore I think I do not have this caps parameter given (or is there a way to get it from vlc?). The stream is given in an mpegts-container.
Here is my latest try:
gst-launch udpsrc uri="udp://239.255.1.1:5005/255" caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)MP4V-ES, profile-level-id=(string)1" ! rtpmp2tdepay ! decodebin ! queue ! TIDmaiVideoSink useUserptrBufs=true numBufs=3 videoStd=720P_60 videoOutput=component sync=false hideOSD=true -v
I would appreciate any help. If you need further information, don't hesitate to ask!
Many thanks in advance!
Gustav