Part Number: AM625
Other Parts Discussed in Thread: ADS7846
Tool/software:
Hello TI
The version of SDK I use:ti-processor-sdk-linux-rt-am62xx-evm-09.02.01.09
I refer to the following link to configure HDMI audio and find the following error:
e2e.ti.com/.../processor-sdk-am62x-about-the-sii9022-hdmi-audio-problem


Here is my device tree configuration:
/*
* Copyright (C) 2015 GuangZhou Tronlong co., LTD - http://www.tronlong.com
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/dts-v1/;
#include "tl62x-evm.dts"
/ {
compatible = "ti,am625-sk", "ti,am625";
model = "TL62x-EVM";
hdmi_mstrclk: hdmi-mstrclk {
compatible = "fixed-clock";
#clock-cells = <0>;
clock-frequency = <24576000>;
};
hdmi: connector {
compatible = "hdmi-connector";
label = "hdmi";
type = "a";
port {
hdmi_connector_in: endpoint {
remote-endpoint = <&sii9022_out>;
};
};
};
hdmi_audio:sound-sii9022 {
compatible = "simple-audio-card";
simple-audio-card,name = "AM62x-Sii9022-HDMI";
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-master = <&hdmi_dailink_master>;
simple-audio-card,frame-master = <&hdmi_dailink_master>;
simple-audio-card,mclk-fs = <2182>;
hdmi_dailink_master:simple-audio-card,cpu {
sound-dai = <&mcasp1>;
system-clock-frequency = <24000000>;
system-clock-direction-out;
};
simple-audio-card,codec {
sound-dai = <&sii9022>;
};
};
};
&codec_audio {
status = "disabled";
};
&main_pmx0 {
main_mcasp1_pins_default: main-mcasp1-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x0024, PIN_INPUT, 2) /* (H25) OSPI0_D6.MCASP1_ACLKX */
AM62X_IOPAD(0x0028, PIN_INPUT, 2) /* (J22) OSPI0_D7.MCASP1_AFSX */
AM62X_IOPAD(0x0020, PIN_OUTPUT, 2) /* (J25) OSPI0_D5.MCASP1_AXR0 */
>;
};
};
&main_i2c2 {
sii9022: sii9022@3b {
#sound-dai-cells = <0>;
compatible = "sil,sii9022";
reg = <0x3b>;
clocks = <&hdmi_mstrclk>;
clock-names = "mclk";
sil,i2s-data-lanes = < 0 >;
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
sii9022_in: endpoint {
remote-endpoint = <&dpi1_out>;
};
};
port@1 {
reg = <1>;
sii9022_out: endpoint {
remote-endpoint = <&hdmi_connector_in>;
};
};
};
};
};
&dss_ports {
/* VP2: DPI Output */
port@1 {
reg = <1>;
dpi1_out: endpoint {
remote-endpoint = <&sii9022_in>;
};
};
};
&lcd0 {
/delete-node/ port;
};
&main_spi0 {
/delete-node/ ads7846@0;
};
&mcasp1 {
status = "okay";
#sound-dai-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&main_mcasp1_pins_default>;
op-mode = <0>; /* MCASP_IIS_MODE */
tdm-slots = <2>;
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
1 0 2 0
0 0 0 0
0 0 0 0
0 0 0 0
>;
tx-num-evt = <0>;
rx-num-evt = <0>;
};
There seems to be a problem with the clock frequency configuration, but it works for me on the processor_sdk_08_06_00_42 version.I hope you can help.