This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM69: WKUP_LF_CLKIN and LFOSC

Part Number: AM69

Tool/software:

Hello,

the LFOSC used in "Table 5-34. Clock Mapping" of the TRM (spruj52c) is referring to WKUP_LF_CLKIN? Is it called LFXOSC_CLKOUT in the registers excel file?

And:

CLK_32K and WKUP_LF_CLKIN are just two separate clocks and I have to select which clock to use peripheral by peripheral (eg. I can select CLK_32K for MCU_TIMER_0 and I can select WKUP_LF_CLKIN for MCU_TIMER_2 based on register configuration).

Kind regards,

Emanuele