This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L137: Enabling EMIFB in PSC1

Part Number: OMAP-L137

Tool/software:

Hello,

I am having problems debugging a board based on OMAP-L137. I am trying to debug the CCS project using the the gel file.

I localized the problem in the gel file, at the EMIFB (SDRAM interface) settings – see below.

I know, the problem appear when setting the EMIFB in PSC1 because when I comment it (see below), I don’t get an error. Anyway, because the EMIFB is not set, another error appear after this, when the SDRAM is used.

 What is causing this problem and how can I fix it?

Regards,

Marius Raducanu

Screenshot of the Console, showing the error when the EMIFB in PSC1 is set:

 

Screenshot of the gel file with the EMIFB setting commented:

Screenshot of the PSC1 table: