Now i can change resolution by passing "omapfb.mode=dvi:1024x768MR-24@60" to kernel, but i want to change resolution when system is running.
How can i do ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Srilatha,
thanks for you advice.
when I just change timing by "echo "39272,800/40/80/128,600/1/23/4" > /sys/devices/platform/omapdss/display0/timings" in X windows, the screen become muss, so I set framebuffer by "fbset -fb /dev/fb0 -xres 800 -yres 600" as you suggestted, but It's not full screen.
I think I should use the tool which X desktop offered to change resolution, such as "xfce4-display-settings".
maybe i should change the title to "how can i change resolution in X windows without reboot system".