Part Number: TDA4VH-Q1
Tool/software:
SDK:ti-processor-sdk-linux-adas-j784s4-evm-09_02_00_05
CPU:TDA4VH-Q1
whe I use SDK 8.5.0 tiboot3.bin can read spi nor falsh ID
when I update sdk to 9.2.0 ;I put tiboot3.bin to nor flash (offset 0x0000 )
but the ID is FF.
how can I config uboot or dts ?
U-Boot SPL 2023.04 (May 29 2024 - 13:45:36 +0800)
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)')
ECC is enabled, priming DDR which will take several seconds.
ECC: priming DDR completed in 2229 msec
SPL initial stack usage: 13456 bytes
Trying to boot from SPI
===>*spi_nor_read_id core
--->spi_nor_read_reg
jedec_spi_nor flash@0: -->unrecognized JEDEC id bytes: ff, ff, ff
SPI probe failed.
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###