Other Parts Discussed in Thread: TMDS64EVM, , AM6442
Tool/software:
reference Use USB in Device Mode (ti.com) on AM64x Academy 9.01.00.00 v1
1) The Use USB in Device Mode section is geared toward the TMDS64EVM (replacement of the GP version) and use of the micro-B connectors.
We should have caveats implemented for the SK-AM64B micro-B connectors, BUT also we really could use implementation references for the SK-AM64B's Type A connector (ref des J7 on the BOM)
2) For the same SK-AM64B's Type A connector (ref des J7)
we should add a "Use USB 3.0 in Host Mode on the AM64x Academy 9.x for an A53 controlled HOST.