Part Number: AM5728
Other Parts Discussed in Thread: SYSBIOS,
Tool/software:
SDK Linux -06.03.00.106
SDK RTOS -06.03.00.106
Running Linux on host and BIOS-RTOS on DSP1 and DSP2. I have built and run the ex02_messageq example successfully
I've been trying to understand the following section of the Dsp2.cfg file of the ex02_messageq example. I have read what documentation I can find on the modules in the examples but its more reference and doesnt give much context of why?
- Is this specifying that the clock ticks are provide by user code?
- Why is timer being created here?
- Is there not a timer built into the RTOS?
- Without this timer would a Task_sleep or a wait on a message queue with timeout work?
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
Clock.tickSource = Clock.TickSource_USER;
var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
/* Skip the Timer frequency verification check. Need to remove this later */
Timer.checkFrequency = false;
/* Match this to the SYS_CLK frequency sourcing the dmTimers.
* Not needed once the SYS/BIOS family settings is updated. */
Timer.intFreq.hi = 0;
Timer.intFreq.lo = 19200000;
var timerParams = new Timer.Params();
timerParams.period = Clock.tickPeriod;
timerParams.periodType = Timer.PeriodType_MICROSECS;
/* Switch off Software Reset to make the below settings effective */
timerParams.tiocpCfg.softreset = 0x0;
/* Smart-idle wake-up-capable mode */
timerParams.tiocpCfg.idlemode = 0x3;
/* Wake-up generation for Overflow */
timerParams.twer.ovf_wup_ena = 0x1;
/* Create Timer module */
Timer.create(Clock.timerId, Clock.doTick, timerParams);
The second set of questions are regarding the idle loop
- Why is the purpose of including the power management module in this example?
- Where is the function IpcPower_idle defined?
/*
* ======== Power Management Configuration ========
*/
/* Bring in modules used in Power Management */
xdc.loadPackage('ti.pm');
var Power = xdc.useModule('ti.sysbios.family.c66.vayu.Power');
Power.loadSegment = "PM_DATA";
/*
* Workaround for silicon bug
*
* IpcPower_callIdle must be placed in L2SRAM and not external memory
* to avoid CPU hang when going into idle. We do so by adding an entry
* into the resource table so that the loader can load to internal L2.
*/
Program.sectMap[".text:IpcPower_callIdle"] = "L2SRAM";
/*
* Add function to support Power Management in the Idle loop
* Must be added after all other Idle functions
*/
Idle.addFunc('&IpcPower_idle');