This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6422: USB root hub support

Part Number: AM6422

Tool/software:

Hi,

Couple of questions on AM64x USB support, as AM64x supports up to 64 slots and has root hub capability:

  1. Details on hardware considerations when connecting more than one device to port.
  2. If I have connected two ports, one to USB device and one to cellular modem, I can still boot from USB at startup (assuming by boot pins are set to USB host)?  Or additional USB switches are needed?

Regards,

Harsha