This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AEN-Q1: Inquiry regarding Crystal PCB Layout in Multi-layer Configuration

Part Number: TDA4AEN-Q1

Tool/software:

Hello! I'd like to inquire about the detailed PCB LAYOUT of the Crystal block in a Multi Layer (2 or more layers).

As far as I know, there are about three important points, as follows:

  1. When using a Ground barrier structure to isolate the Crystal, it's preferable to connect the Ground behind the Ground pin of the AP's Crystal with a single Via.

  2. In a Multi-layer configuration, the bottom of the Crystal should be all Ground with no signal lines, and only the bottom layer should have a Ground Plane to shield against EMI.

  3. The Ground path of External Capacitors should be kept as short as possible.

Now, let's consider the case mentioned above. Although it's a 6-layer PCB, for convenience, only 4 layers have been captured.

Question 1: Looking at the Top Layer, there is only one GND pin next to the XTAl pin, with a single via created next to it. In this case, wouldn't the Ground path of the Capacitor above the Top Layer become too long, causing an issue?

Question 2: The 2-layer setup has a clean Ground Plane. Doesn't this mean that ultimately there's no point in isolating on the Top layer? Shouldn't the isolation be the same for both layers? Like this:

Let me show you one more example. Although the diagram shows a 10-layer structure, only the layout of 4 layers has been brought.

Question 3: Why wasn't Ground isolated in this case? When is it better not to isolate?

Question 4: In the 3-layer setup, some signals including I2C Clk are passing through. Although they are not high-speed signals, does it matter since there is a Ground plane on the 2nd layer?

I apologize for the lengthy text, but the core of what I want to know is as follows:

Common Question 1: When grounding isolation, what is the most ideal number and placement of vias?

Common Question 2: When grounding isolation, is it better to eliminate even the Ground Plane on the 2nd layer or other inner layers?

Common Question 3: If there are power or signal lines on the 3rd layer and Ground plane must be placed on the 2nd layer, should this plane also be isolated?

I would greatly appreciate detailed explanations. There is no proper explanation in any of TI's Crystal PCB layout Guides.

  • Especially, I'm keen to know the following points (reiterated for clarity due to the length of the text):

    When isolating the Ground of the Crystal block on the Top Layer in a Multi-layer setup, how should the Inner layers be managed?

    1: Is it advisable to keep all layers, except the Bottom Layer, as a keep-out zone?

    2: If, due to spatial limitations, signal/power lines must unavoidably traverse an Inner layer, requiring the use of a Ground plane on the 2nd Layer, should this Ground Plane be isolated everywhere except for vias, akin to the Top layer?

  • The TDA4AEN-Q1 package does NOT have a dedicated GND pin, thus the amount of isolation that can be done is limited.  The recommendation is to keep GND simple and combine all GNDs.  This provides over-all lowest impedance for GND (which is good) and keeps possible mistakes from being made.  If high current return paths are a concern - then power supply components/capacitors can be placed strategically to minimize high current paths in area of crystal.  If you wish to further isolate, then can use a separate GND and connect at single point near processor (example at processor GND pin).  But again - processor does not have dedicated GND pin for crystal - but could use GND pin closes to XTAL pins.