I am working on using the previewer with input taken directly from the ccdc on a dm6435. I am getting an output image, but I am not sure if the resulting image width is correct. I am acquiring an image that is 1280 pixels wide in raw bayer format. I expect to lose 4 pixels from cfa interpolation in the previewer. All of the other previewer features have been disabled. But instead of getting 1276 active pixels out, I am getting 1272 good pixels out (the output line offset is 1280 pixels to meet 32 byte alignment requirements.) The documentation (spru977d, section 5.5.6) says that I have to set the previewer starting pixel to a minimum of 2 and the ending pixel to at least 2 from the end when the input is taken from the ccdc. Am I supposed to lose those 4 pixels in addition to the 4 pixels lost to cfa interpolation by the previewer?