Other Parts Discussed in Thread: OMAP-L137
Hi,
recently I was able to build and successfully run the OMAPL137_AM17X_SAMPLE on the OMAP L137 EVM of Spectrum Digital Inc
Today I wanted to run it standalone and copied the RELEASE image nk.nb0 to the preformatted (FAT32) SD-card ( as described in the Quick-Start-Guide ).
After having configured EBOOT to boot from SD-card, it seemed to work perfectly but shortly before beeing ready ( it is at the line " KITL: using sysintr 0x11" ) it paused for about 100 sec. , then continued with the rest but finally did not respond to any Ping from outside.
Any idea what does not work here ?
Output from the serial port:
************************************************************************************************************
Booting with TI UBL
Device OPP (300MHz, 1.2V)01
Microsoft Windows CE Bootloader Common Library Version 1.4 Built Aug 17 2011 21:
18:23
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
Microsoft Windows CE EBOOT 1.0 for OMAPL137 OMAPL137/AM17X EVM. Built Aug 17 201
1 at 21:24:59
BSP version 01.10.00, SOC version 01.10.00
CODE : 0xC3F60000 -> 0xC3FA0000
DATA : 0xC3FA0000 -> 0xC3FE0000
STACK : 0xC3FE0000 -> 0xC3FF9800
Enabled OAL Log Zones : ERROR, WARN, INFO,
Platform Init done
System ready!
Preparing for download...
Predownload...
Valid boot configuration found
fetch_production_data: MAC-1 00:0e:99:03:14:82
fetch_production_data: MAC-2 00:0e:99:03:14:83
INFO: MAC address: 00:0e:99:03:14:82
WARN: Invalid BSP_ARGS data found (using defaults)
WARN: Unable to get hardware entropy
Hit space to enter configuration menu 0
Device ID set to hallo-omap
BLFlashDownload: LogicalLoc - 0x01C40000
Loading from SD card
+ReadNKFromSDMMC
ReadFileFromSDMMC: reading file 'nk.bin'
SDBootPDD: PDD_SDInitializeHardware: MMCSD
SDBootMDD: SDInitializeHardware: SD card detected
SDBootMDD: SDInitializeHardware: V2.0 card detected
SDBootMDD: SDInitializeHardware: timeOut = 0
SDBootMDD: SDInitializeHardware: timeOut = 1
SDBootMDD: SDInitializeHardware: timeOut = 2
SDBootMDD: SDInitializeHardware: timeOut = 3
SDBootMDD: Card address is aaaa
SDBootMDD: 4-bit data bus selected
InitMasterBootRecord: Partition 0, type 11
InitMasterBootRecord: Partition 0, FAT32, start 0x10e00, length 0x75c07200
InitPartition: Offset 0x10e00, length 0x75c07200
ReadFileFromSDMMC: can't open image file 'nk.bin'
ReadFileFromSDMMC: reading file 'nk.nb0'
SDBootPDD: PDD_SDInitializeHardware: MMCSD
SDBootMDD: SDInitializeHardware: SD card detected
SDBootMDD: SDInitializeHardware: V2.0 card detected
SDBootMDD: SDInitializeHardware: timeOut = 0
SDBootMDD: SDInitializeHardware: timeOut = 1
SDBootMDD: Card address is f551
SDBootMDD: 4-bit data bus selected
InitMasterBootRecord: Partition 0, type 11
InitMasterBootRecord: Partition 0, FAT32, start 0x10e00, length 0x75c07200
InitPartition: Offset 0x10e00, length 0x75c07200
ReadFileFromSDMMC: file size = 33554432 bytes
CheckCEImage: checking image at 0xc0000000
ROMHDR (pTOC = 0xc0da8130) ---------------------
DLL First : 0x4001c001
DLL Last : 0x408ec094
Physical First : 0x80000000
Physical Last : 0x80f28940
Num Modules : 169
RAM Start : 0x80f30000
RAM Free : 0x810fe000
RAM End : 0x8373f800
Num Copy Entries : 4
Copy Entries Offset : 0x809ef8ac
Prof Symbol Length : 0x0017eb2c
Prof Symbol Offset : 0x80f7f000
Num Files : 68
Kernel Flags : 0x00000000
FileSys RAM Percent : 0x30303030
Driver Glob Start : 0x00000000
Driver Glob Length : 0x00000000
CPU : 0x01c2
MiscFlags : 0x0002
Extensions : 0x80001070
Tracking Mem Start : 0x00000000
Tracking Mem Length : 0x00000000
------------------------------------------------
Image Start .......: 0x00000000
Image Size ........: 0x00000000
Image Launch Addr .: 0x00000000
Image ROMHDR ......: 0x00000000
Boot Device/Type ..: 3 / 6
INFO: Launch Windows Embedded CE by jumping to 0xc0000000...
ADE
Windows CE Kernel for ARM (Thumb Enabled) Built on Nov 3 2010 at 07:30:04
OEMInit: init.c built on Aug 17 2011 at 21:25:30.
BSP version 01.10.00, SOC version 01.10.00
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xf
WARN: Updating local copy of BSP_ARGS
Intr Init done...
Timer Init done...
+OALDumpClocks
Clock Configuration :
Reference Clock 0 .. 24000000 Hz
PLL0 ............. 300000000 Hz
PLL0:SYSCLK1 ..... 300000000 Hz (DSP Subsystem)
PLL0:SYSCLK2 ..... 150000000 Hz (UART,EDMA,SPI,MMC/SD,eCAP,eQEP,ePWM,LCDC,HP
I,McASP,EMIFB)
PLL0:SYSCLK3 ..... 100000000 Hz (EMIFA)
PLL0:SYSCLK4 ..... 75000000 Hz (INTC, SYSCFG, PSC, I2C1, USB1.1, EMAC/MDIO,
GPIO)
PLL0:SYSCLK5 ..... 50000000 Hz (EMIFB I/O clock)
PLL0:SYSCLK6 ..... 300000000 Hz (ARM Subsystem)
PLL0:SYSCLK7 ..... 50000000 Hz (EMAC)
PLL0:AUXCLK ...... 24000000 Hz (I2C0, Timers, McASP serial clock, RTC, USB2
.0)
-OALDumpClocks
WARN: Updating local copy of BSP_ARGS
OEMKitlStartup(mac = 00:0e:99:03:14:82)
DeviceId................. hallo-omap
pArgs->flags............. 0xD
pArgs->devLoc.IfcType.... 0
pArgs->devLoc.LogicalLoc. 0x1E23000
pArgs->devLoc.PhysicalLoc 0x0
pArgs->devLoc.Pin........ 0
pArgs->ip4address........ 0
pDevice->Name............ s
pDevice->ifcType......... 0
pDevice->id.............. 0x1E23000
pDevice->resource........ 0
pDevice->type............ 2
pDevice->pDriver......... 0x80F39000
MAC addr is 0:e:99:3:14:82.
OMAPEmacInit: f_pEmacRxDesc = 0xb0620000
OMAPEmacInit: f_pEmacTxDesc = 0xb0621000
OMAPEmacInit: waiting for active phy...
OMAPEmacInit: f_pMdioRegs->m_Alive = 0xe
KITL: *** Device Name hallo-omap ***
KITL: using sysintr 0x11 <------- HERE IT PAUSED FOR 100 sec. !!!!
VBridge:: built on [Sep 6 2006] time [19:28:11]
VBridgeInit()...TX = [16384] bytes -- Rx = [16384] bytes
Tx buffer [0xA0F6FCA0] to [0xA0F73CA0].
Rx buffer [0xA0F73CC0] to [0xA0F77CC0].
VBridge:: NK add MAC: [0-E-99-3-14-82]
ERROR: OALKitlInit: KitlInit failed
-OEMInit
PINMUX8 =0x21122111
PINMUX9 =0x00008412
PINMUX10=0x22222220
PINMUX11=0x00000022
PINMUX12=0x00000000
PINMUX13=0x22111100
PINMUX14=0x44222222
PINMUX15=0x22444444
PINMUX16=0x22222222
PINMUX17=0x80822282
PINMUX18=0x08000008
PINMUX19=0x00000000
CFGCHIP1=0x00000000
CFGCHIP2=0x00008a82
OEMGetExtensionDRAM: Added 0x83E00000 -> 0x84000000
WARN: Updating local copy of BSP_ARGS
OEM: Cleaning system hive
OEM: Cleaning user profiles
WARN: Updating local copy of BSP_ARGS
OEM: Not cleaning system hive
VBridge:: VB_INITIALIZED returns [1]
VBridge:: RESET_BUFFER received.
**************************************************************************
System is not reachable over Ping !
Best regards,
Franz