This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM35x-OMAP35x-LINUX-PSP-04.02.00.07 hangsout

Other Parts Discussed in Thread: DM3730

i have tried the psp 03 version its work fine in MIstral DM3730 evm

but according to the link

          http://processors.wiki.ti.com/index.php/GSG:_AM35x_and_OMAP35x_Graphics_SDK_Additional_Procedures

           we need to use psp 04 version we can use the DVI output.

so , i have downloaded the psp version 04 from from the link

          http://software-dl.ti.com/dsps/dsps_public_sw/psp/LinuxPSP/OMAP_04_02/04_02_00_07//exports/AM35x-OMAP35x-LINUX-PSP-04.02.00.07.tgz 

so i go for the making 3 partion on sd card fro this link

         http://processors.wiki.ti.com/index.php/How_to_Make_3_Partition_SD_Card

 

after all this i have done.

in minicom

Texas Instruments X-Loader 1.51 (May  3 2011 - 19:22:23)                       
Starting X-loader on MMC                                                       
Reading boot sector                                                            
                                                                               
220008 Bytes Read from MMC                                                     
Starting OS Bootloader from MMC...                                             
Starting OS Bootloader...                                                      
                                                                               
                                                                               
U-Boot 2010.06 (May 03 2011 - 19:23:34)                                        
                                                                               
OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz                                     
OMAP3 EVM board + LPDDR/NAND                                                   
I2C:   ready                                                                   
DRAM:  256 MiB                                                                 
NAND:  HW ECC [Kernel/FS layout] selected                                      
512 MiB                                                                        
Error: Bad compare! failed                                                     
Error: Bad compare! failed                                                     
Error: Bad compare! failed                                                     
Error: Bad compare! failed                                                     
*** Warning - bad CRC or NAND, using default environment                       
                                                                               
In:    serial                                                                  
Out:   serial                                                                  
Err:   serial                                                                  
Read back SMSC id 0x92200000                                                   
Die ID #35d400029ff800000160716408020009                                       
Net:   smc911x-0                                                               
Hit any key to stop autoboot:  0                                               
mmc1 is available                                                              
reading boot.scr                                                               
                                                                               
** Unable to read "boot.scr" from mmc 0:1 **                                   
reading uImage                                                                 
                                                                               
3082808 bytes read                                                             
Booting from mmc ...                                                           
## Booting kernel from Legacy Image at 82000000 ...                            
   Image Name:   Linux-2.6.37-14270-gadcd067                                   
   Image Type:   ARM Linux Kernel Image (uncompressed)                         
   Data Size:    3082744 Bytes = 2.9 MiB                                       
   Load Address: 80008000                                                      
   Entry Point:  80008000                                                      
   Verifying Checksum ... OK                                                   
   Loading Kernel Image ... OK                                                 
OK                                                                             
                                                                               
Starting kernel ...                                                            
                                                                               
Uncompressing Linux... done, booting the kernel.                               
[    0.000000] Linux version 2.6.37-14270-gadcd067 (x0029463@psplinux050) (gcc 1
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f 
[    0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: OMAP3 EVM                                              
[    0.000000] Reserving 4194304 bytes SDRAM for VRAM                          
[    0.000000] Memory policy: ECC disabled, Data cache writeback               
[    0.000000] OMAP3630 ES1.2 (l2cache i

.................

.................                     after all initalising process

................

onfiguring kernel-module-cryptodev.                                           
Configuring kernel-module-output.                                              
Configuring kernel-module-scsi-wait-scan.                                      
Configuring ti-ocf-crypto-module.                                              
Configuring kernel-image-2.6.32.                                               
INIT: Entering runlevel: 5                                                     
Starting system message bus: dbus.                                             
Creating Dropbear SSH server RSA host key.                                     
Will output 1024 bit rsa secret key to '/etc/dropbear/dropbear_rsa_host_key'   
Generating key, this may take a while...                                       
Public key portion is:                                                         
ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAAAgwCzw05x2CT+gYMSAlAg7ngGtKkp6qJbUt3en3ZvZ3Vm
Fingerprint: md5 39:5e:22:e9:57:18:c1:27:e1:a6:1a:95:6c:b1:e4:12               
Starting Dropbear SSH server: dropbear.                                        
Starting telnet daemon.                                                        
Starting syslogd/klogd: done                                                   
Starting thttpd.                                                               
Starting PVR                                                                   
Usage: insmod filename [args]                                                  
FATAL: Module omaplfb not found.                                               
FATAL: Module bufferclass_ti not found.                                        
BusyBox v1.13.2 (2010-12-19 17:09:32 CST) multi-call binary                    
                                                                               
Usage: mknod [OPTIONS] NAME TYPE MAJOR MINOR                                   
                                                                               
Create a special file (block, character, or pipe)                              
                                                                               
Options:                                                                       
        -m      Create the special file using the specified mode (default a=rw)
TYPEs include:                                                                 
        b:      Make a block device                                            
        c or u: Make a character device                                        
        p:      Make a named pipe (MAJOR and MINOR are ignored)                
                                                                               
chmod: /dev/pvrsrvkm: No such file or directory                                
Starting SGX fixup for ES5.x                                                   
Calibrating touchscreen (first time only)xres = 480, yres = 640                
selected device is not a touchscreen I understand                              
Took 2 samples...                                                              
Top left : X = -545451948 Y = -545451825                                       
Took 2 samples...                                                              
Top right : X = -545451948 Y = -545451825                                      
Took 2 samples...                                                              
Bot right : X = -545451948 Y = -545451825                                      
Took 2 samples...                                                              
Bot left : X = -545451948 Y = -545451825                                       
Took 2 samples...                                                              
Center : X = -545451948 Y = -545451825                                         
0.625983 -0.000007 0.000007                                                    
0.309701 -0.000009 0.000009                                                    
Calibration constants: 41024 0 0 20296 0 0 65536                               
.                                                                              
Starting Matrix GUI application.                                               
                                                                               
[   92.057525] mmcblk0: error -110 transferring data, sector 1849050, nr 8, car0
[   92.079498] end_request: I/O error, dev mmcblk0, sector 1849051             
[   92.085723] Buffer I/O error on device mmcblk0p2, logical block 211050      
[   92.092559] lost page write due to I/O error on mmcblk0p2                   
[   98.451629] mmcblk0: error -110 sending read/write command, response 0x900, 0
[   98.460662] mmcblk0: error -110 transferring data, sector 692626, nr 72, car0
[   98.501373] end_request: I/O error, dev mmcblk0, sector 692627              
[   98.507507] end_request: I/O error, dev mmcblk0, sector 692634              
[   98.513641] end_request: I/O error, dev mmcblk0, sector 692642              
[   98.519775] end_request: I/O error, dev mmcblk0, sector 692650              
[   98.525878] end_request: I/O error, dev mmcblk0, sector 692658              
[   98.532012] end_request: I/O error, dev mmcblk0, sector 692666              
[   98.538146] end_request: I/O error, dev mmcblk0, sector 692674              
[   98.544250] end_request: I/O error, dev mmcblk0, sector 692682              
[   98.550384] end_request: I/O error, dev mmcblk0, sector 692690              
[   98.556823] Aborting journal on device mmcblk0p2.                           
[   98.561981] EXT3-fs (mmcblk0p2): error in ext3_reserve_inode_write: Journal d
[   99.516113] EXT3-fs (mmcblk0p2): error in ext3_dirty_inode: Journal has abord
[   99.968780] EXT3-fs (mmcblk0p2): error: ext3_journal_start_sb: Detected aborl
[   99.977294] EXT3-fs (mmcblk0p2): error: remounting filesystem read-only     
INIT: Id "S" respawning too fast: disabled for 5 minutes                       
INIT: Id "S" respawning too fast: disabled for 5 minutes                       
INIT: Id "S" respawning too fast: disabled for 5 minutes    

 

 

it comes like that

the matrix screen appears

but touch fails to work..

i have paste the u-boot,u images and x-loader given in prebuilt images.....

is any other ideas.....