Dear all,
I'm having real difficulties with the DM816x EVM board with USB.
USB with DMA enabled seems to be just about completely broken and useless. I get some short periods of correct behaviour, then 'something' stops working.
With PIO selected instead of DMA, things are ok until I start transferring higher data rates... then it all dies yet again.
Behaviour is better with a memory stick than it is with a Wifi device.
I'm using the latest PSP (4.0.0.12) / EZSDK release.
I'm a little concerned that I see postings from Ajay Kumar Gupta to the linux-wireless dev list, adding what looks like tentative PIO-only single-port-only support for this USB host controller.
Could someone maybe enlighten me to the status of USB for the DM816x series, as it currently appears to be rather bad and unfit for production just now.
Many thanks,
Ian.