Part Number: TDA4VM
Tool/software:
Hi,
The timer module in TDA4x devices provides an option to cascade the timers. Each odd numbered timer instance from each of the domain may be optionally cascaded with previous even numbered timer instance for the same domain to form up to a 64-bit timer. When cascaded, TIMER_i acts as a 32- bit pre scaler to TIMER_1+1
I am trying to implement the feature with the below implementation:
/* ========================================================================== */
/* Include Files */
/* ========================================================================== */
#include <stdint.h>
#include <ti/board/board.h>
#include <ti/drv/uart/UART.h>
#include <ti/drv/uart/UART_stdio.h>
#include <ti/csl/cslr.h>
/* ========================================================================== */
/* Macros & Typedefs */
/* ========================================================================== */
/* None */
/* ========================================================================== */
/* Structure Declarations */
/* ========================================================================== */
/* None */
/* ========================================================================== */
/* Function Declarations */
/* ========================================================================== */
#define CTRL_MMR_CAP_SEL 0x40F04204
#define TIMER2_TLDR 0x40410040
#define TIMER2_TWPS 0x40410048
#define TIMER2_TCLR 0x40410038
#define TIMER2_TTGR 0x40410044
#define TIMER2_TCRR 0x4041003C
#define TIMER1_TLDR 0x40400040
#define TIMER1_TWPS 0x40400048
#define TIMER1_TTGR 0x40400044
#define TIMER1_TCLR 0x40400038
#define TIMER1_TCRR 0x4040003C
/* ========================================================================== */
/* Global Variables */
/* ========================================================================== */
/* None */
/* ========================================================================== */
/* Function Definitions */
/* ========================================================================== */
//Timer 2 should start counting when timer 1 overflows
int main(void)
{
Board_initCfg boardCfg;
boardCfg = BOARD_INIT_UNLOCK_MMR |
BOARD_INIT_MODULE_CLOCK |
BOARD_INIT_PINMUX_CONFIG |
BOARD_INIT_UART_STDIO;
Board_init(boardCfg);
volatile uint32_t twps_val = 1;
volatile uint32_t timer2;
volatile uint32_t timer1;
UART_printf("Cascaded Timer Test\n");
UART_printf("Enabling Cascade\n");
CSL_REG32_WR(CTRL_MMR_CAP_SEL, 0x100);
UART_printf("Setting up timer 2\n");
CSL_REG32_WR(TIMER2_TLDR, 0xFFFFFFF0);
CSL_REG32_WR(TIMER2_TTGR, 0x20);
CSL_REG32_WR(TIMER2_TCLR, 0x1);
UART_printf("Checking write posted for TCLR2\n");
twps_val = CSL_REG32_RD(TIMER2_TWPS);
while(twps_val == 0x1)
{
twps_val = CSL_REG32_RD(TIMER2_TWPS);
}
UART_printf("Setting up timer 1\n");
CSL_REG32_WR(TIMER1_TLDR, 0xF0000000);
CSL_REG32_WR(TIMER1_TTGR, 0x20);
CSL_REG32_WR(TIMER1_TCLR, 0x403);
UART_printf("Checking TWPS Val\n");
while(twps_val == 0x1)
{
twps_val = CSL_REG32_RD(TIMER1_TWPS);
}
while(1)
{
timer1 = CSL_REG32_RD(TIMER1_TCRR);
timer2 = CSL_REG32_RD(TIMER2_TCRR);
UART_printf("TIMER1 = 0x%x, TIMER2 = 0x%x\n", timer1, timer2);
}
return(0);
}
Please see the logs attached from the above code.
SBL Revision: 01.00.10.01 (Jul 27 2023 - 17:57:55) TIFS ver: 9.0.6--v09.00.06 (Kool Koala) Cascaded Timer Test Enabling Cascade Setting up timer 2 Checking write posted for TCLR2 Setting up timer 1 Checking TWPS Val TIMER1 = 0xf04c63f3, TIMER2 = 0x0 TIMER1 = 0xf0d5ecef, TIMER2 = 0x0 TIMER1 = 0xf15f6e23, TIMER2 = 0x0 TIMER1 = 0xf1e8ef45, TIMER2 = 0x0 TIMER1 = 0xf272706d, TIMER2 = 0x0 TIMER1 = 0xf2fbf18f, TIMER2 = 0x0 TIMER1 = 0xf38572b7, TIMER2 = 0x0 TIMER1 = 0xf40ef3df, TIMER2 = 0x0 TIMER1 = 0xf4987501, TIMER2 = 0x0 TIMER1 = 0xf521f623, TIMER2 = 0x0 TIMER1 = 0xf5ab7751, TIMER2 = 0x0 TIMER1 = 0xf634f879, TIMER2 = 0x0 TIMER1 = 0xf6be79a1, TIMER2 = 0x0 TIMER1 = 0xf747fac3, TIMER2 = 0x0 TIMER1 = 0xf7d17beb, TIMER2 = 0x0 TIMER1 = 0xf85afd19, TIMER2 = 0x0 TIMER1 = 0xf8e47e41, TIMER2 = 0x0 TIMER1 = 0xf96dff63, TIMER2 = 0x0 TIMER1 = 0xf9f7808b, TIMER2 = 0x0 TIMER1 = 0xfa8101a7, TIMER2 = 0x0 TIMER1 = 0xfb0a82c9, TIMER2 = 0x0 TIMER1 = 0xfb9403f1, TIMER2 = 0x0 TIMER1 = 0xfc1d8519, TIMER2 = 0x0 TIMER1 = 0xfca70641, TIMER2 = 0x0 TIMER1 = 0xfd308769, TIMER2 = 0x0 TIMER1 = 0xfdba0897, TIMER2 = 0x0 TIMER1 = 0xfe4389b9, TIMER2 = 0x0 TIMER1 = 0xfecd0ae1, TIMER2 = 0x0 TIMER1 = 0xff568c03, TIMER2 = 0x0 TIMER1 = 0xffe00d37, TIMER2 = 0x0 TIMER1 = 0xf0698e65, TIMER2 = 0x0 --------------------> 1st OverFlow TIMER1 = 0xf0f30f93, TIMER2 = 0x0 TIMER1 = 0xf17c90bb, TIMER2 = 0x0 TIMER1 = 0xf20611e9, TIMER2 = 0x0 TIMER1 = 0xf28f9317, TIMER2 = 0x0 TIMER1 = 0xf319143f, TIMER2 = 0x0 TIMER1 = 0xf3a29567, TIMER2 = 0x0 TIMER1 = 0xf42c168f, TIMER2 = 0x0 TIMER1 = 0xf4b597b1, TIMER2 = 0x0 TIMER1 = 0xf53f18df, TIMER2 = 0x0 TIMER1 = 0xf5c89a07, TIMER2 = 0x0 TIMER1 = 0xf6521b29, TIMER2 = 0x0 TIMER1 = 0xf6db9c51, TIMER2 = 0x0 TIMER1 = 0xf7651d73, TIMER2 = 0x0 TIMER1 = 0xf7ee9e9b, TIMER2 = 0x0 TIMER1 = 0xf8781fc3, TIMER2 = 0x0 TIMER1 = 0xf901a0e5, TIMER2 = 0x0 TIMER1 = 0xf98b2207, TIMER2 = 0x0 TIMER1 = 0xfa14a335, TIMER2 = 0x0 TIMER1 = 0xfa9e245d, TIMER2 = 0x0 TIMER1 = 0xfb27a585, TIMER2 = 0x0 TIMER1 = 0xfbb126a7, TIMER2 = 0x0 TIMER1 = 0xfc3aa7cf, TIMER2 = 0x0 TIMER1 = 0xfcc428fd, TIMER2 = 0x0 TIMER1 = 0xfd4daa25, TIMER2 = 0x0 TIMER1 = 0xfdd72b47, TIMER2 = 0x0 TIMER1 = 0xfe60ac6f, TIMER2 = 0x0 TIMER1 = 0xfeea2d8b, TIMER2 = 0x0 TIMER1 = 0xff73aead, TIMER2 = 0x0 TIMER1 = 0xfffd2fd5, TIMER2 = 0x0 TIMER1 = 0xf086b0fd, TIMER2 = 0x0 --------------------> 2nd OverFlow TIMER1 = 0xf1103225, TIMER2 = 0x0 TIMER1 = 0xf199b34d, TIMER2 = 0x0 TIMER1 = 0xf223347b, TIMER2 = 0x0 TIMER1 = 0xf2acb59d, TIMER2 = 0x0 TIMER1 = 0xf33636c5, TIMER2 = 0x0 TIMER1 = 0xf3bfb7f3, TIMER2 = 0x0 TIMER1 = 0xf449391b, TIMER2 = 0x0 TIMER1 = 0xf4d2ba49, TIMER2 = 0x0 TIMER1 = 0xf55c3b77, TIMER2 = 0x0 TIMER1 = 0xf5e5bc9f, TIMER2 = 0x0 TIMER1 = 0xf66f3dc7, TIMER2 = 0x0 TIMER1 = 0xf6f8beef, TIMER2 = 0x0 TIMER1 = 0xf7824011, TIMER2 = 0x0 TIMER1 = 0xf80bc13f, TIMER2 = 0x0 TIMER1 = 0xf8954267, TIMER2 = 0x0 TIMER1 = 0xf91ec389, TIMER2 = 0x0 TIMER1 = 0xf9a844b1, TIMER2 = 0x0 TIMER1 = 0xfa31c5d3, TIMER2 = 0x0 TIMER1 = 0xfabb46fb, TIMER2 = 0x0 TIMER1 = 0xfb44c823, TIMER2 = 0x0 TIMER1 = 0xfbce4945, TIMER2 = 0x0 TIMER1 = 0xfc57ca67, TIMER2 = 0x0 TIMER1 = 0xfce14b95, TIMER2 = 0x0 TIMER1 = 0xfd6accbd, TIMER2 = 0x0 TIMER1 = 0xfdf44de5, TIMER2 = 0x0 TIMER1 = 0xfe7dcf07, TIMER2 = 0x0 TIMER1 = 0xff07502f, TIMER2 = 0x0 TIMER1 = 0xff90d15d, TIMER2 = 0x0 TIMER1 = 0xf01a5285, TIMER2 = 0x0 --------------------> 3rd OverFlow TIMER1 = 0xf0a3d3a7, TIMER2 = 0x0 TIMER1 = 0xf12d54cf, TIMER2 = 0x0 TIMER1 = 0xf1b6d5eb, TIMER2 = 0x0 TIMER1 = 0xf2405719, TIMER2 = 0x0 TIMER1 = 0xf2c9d83b, TIMER2 = 0x0 TIMER1 = 0xf3535963, TIMER2 = 0x0 TIMER1 = 0xf3dcda85, TIMER2 = 0x0 TIMER1 = 0xf4665bad, TIMER2 = 0x0 TIMER1 = 0xf4efdcdb, TIMER2 = 0x0 TIMER1 = 0xf5795dfd, TIMER2 = 0x0 TIMER1 = 0xf602df25, TIMER2 = 0x0 TIMER1 = 0xf68c6047, TIMER2 = 0x0 TIMER1 = 0xf715e17b, TIMER2 = 0x0 TIMER1 = 0xf79f62a3, TIMER2 = 0x0 TIMER1 = 0xf828e3c5, TIMER2 = 0x0 TIMER1 = 0xf8b264ed, TIMER2 = 0x0 TIMER1 = 0xf93be609, TIMER2 = 0x0 TIMER1 = 0xf9c5672b, TIMER2 = 0x0 TIMER1 = 0xfa4ee853, TIMER2 = 0x0 TIMER1 = 0xfad8697b, TIMER2 = 0x0 TIMER1 = 0xfb61ea9d, TIMER2 = 0x0 TIMER1 = 0xfbeb6bcb, TIMER2 = 0x0 TIMER1 = 0xfc74ecf3, TIMER2 = 0x0 TIMER1 = 0xfcfe6e1b, TIMER2 = 0x0 TIMER1 = 0xfd87ef43, TIMER2 = 0x0 TIMER1 = 0xfe117071, TIMER2 = 0x0 TIMER1 = 0xfe9af199, TIMER2 = 0x0 TIMER1 = 0xff2472c7, TIMER2 = 0x0 TIMER1 = 0xffadf3f5, TIMER2 = 0x0 TIMER1 = 0xf037751d, TIMER2 = 0x0 --------------------> 4th OverFlow TIMER1 = 0xf0c0f645, TIMER2 = 0x0 TIMER1 = 0xf14a7767, TIMER2 = 0x0 TIMER1 = 0xf1d3f88f, TIMER2 = 0x0 TIMER1 = 0xf25d79bd, TIMER2 = 0x0 TIMER1 = 0xf2e6fae5, TIMER2 = 0x0 TIMER1 = 0xf3707c0d, TIMER2 = 0x0 TIMER1 = 0xf3f9fd2f, TIMER2 = 0x0 TIMER1 = 0xf4837e5d, TIMER2 = 0x0 TIMER1 = 0xf50cff7f, TIMER2 = 0x0 TIMER1 = 0xf59680a7, TIMER2 = 0x0 TIMER1 = 0xf62001cf, TIMER2 = 0x0 TIMER1 = 0xf6a982f1, TIMER2 = 0x0 TIMER1 = 0xf7330419, TIMER2 = 0x0 TIMER1 = 0xf7bc8541, TIMER2 = 0x0 TIMER1 = 0xf8460669, TIMER2 = 0x0 TIMER1 = 0xf8cf8791, TIMER2 = 0x0 TIMER1 = 0xf95908bf, TIMER2 = 0x0 TIMER1 = 0xf9e289e1, TIMER2 = 0x0 TIMER1 = 0xfa6c0b09, TIMER2 = 0x0 TIMER1 = 0xfaf58c37, TIMER2 = 0x0 TIMER1 = 0xfb7f0d5f, TIMER2 = 0x0 TIMER1 = 0xfc088e87, TIMER2 = 0x0 TIMER1 = 0xfc920faf, TIMER2 = 0x0 TIMER1 = 0xfd1b90d1, TIMER2 = 0x0 TIMER1 = 0xfda511ff, TIMER2 = 0x0 TIMER1 = 0xfe2e9327, TIMER2 = 0x0 TIMER1 = 0xfeb81449, TIMER2 = 0x0 TIMER1 = 0xff419571, TIMER2 = 0x0 TIMER1 = 0xffcb1693, TIMER2 = 0x0 TIMER1 = 0xf05497bb, TIMER2 = 0x0 --------------------> 5th OverFlow TIMER1 = 0xf0de18e3, TIMER2 = 0x0 TIMER1 = 0xf1679a05, TIMER2 = 0x0 TIMER1 = 0xf1f11b33, TIMER2 = 0x0 TIMER1 = 0xf27a9c5b, TIMER2 = 0x0 TIMER1 = 0xf3041d83, TIMER2 = 0x0 TIMER1 = 0xf38d9eab, TIMER2 = 0x0 TIMER1 = 0xf4171fd9, TIMER2 = 0x0 TIMER1 = 0xf4a0a101, TIMER2 = 0x0 TIMER1 = 0xf52a2229, TIMER2 = 0x0 TIMER1 = 0xf5b3a34b, TIMER2 = 0x0 TIMER1 = 0xf63d2473, TIMER2 = 0x0 TIMER1 = 0xf6c6a5a1, TIMER2 = 0x0 TIMER1 = 0xf75026c9, TIMER2 = 0x0 TIMER1 = 0xf7d9a7eb, TIMER2 = 0x0 TIMER1 = 0xf8632913, TIMER2 = 0x0 TIMER1 = 0xf8ecaa2f, TIMER2 = 0x0 TIMER1 = 0xf9762b5d, TIMER2 = 0x0 TIMER1 = 0xf9ffac7f, TIMER2 = 0x0 TIMER1 = 0xfa892da7, TIMER2 = 0x0 TIMER1 = 0xfb12aec9, TIMER2 = 0x0 TIMER1 = 0xfb9c2ff1, TIMER2 = 0x0 TIMER1 = 0xfc25b11f, TIMER2 = 0x0 TIMER1 = 0xfcaf3241, TIMER2 = 0x0 TIMER1 = 0xfd38b369, TIMER2 = 0x0 TIMER1 = 0xfdc2348b, TIMER2 = 0x0 TIMER1 = 0xfe4bb5bf, TIMER2 = 0x0 TIMER1 = 0xfed536e7, TIMER2 = 0x0 TIMER1 = 0xff5eb809, TIMER2 = 0x0 TIMER1 = 0xffe83931, TIMER2 = 0x0 TIMER1 = 0xf071ba4d, TIMER2 = 0x1 --------------------> 6th OverFlow TIMER1 = 0xf0fb3b6f, TIMER2 = 0x1 TIMER1 = 0xf184bc97, TIMER2 = 0x1 TIMER1 = 0xf20e3dbf, TIMER2 = 0x1 TIMER1 = 0xf297bee1, TIMER2 = 0x1 TIMER1 = 0xf321400f, TIMER2 = 0x1 TIMER1 = 0xf3aac137, TIMER2 = 0x1 TIMER1 = 0xf434425f, TIMER2 = 0x1 TIMER1 = 0xf4bdc387, TIMER2 = 0x1 TIMER1 = 0xf54744a9, TIMER2 = 0x1 TIMER1 = 0xf5d0c5dd, TIMER2 = 0x1 TIMER1 = 0xf65a4705, TIMER2 = 0x1 TIMER1 = 0xf6e3c827, TIMER2 = 0x1 TIMER1 = 0xf76d494f, TIMER2 = 0x1 TIMER1 = 0xf7f6ca7d, TIMER2 = 0x1 TIMER1 = 0xf8804ba5, TIMER2 = 0x1 TIMER1 = 0xf909ccc7, TIMER2 = 0x1 TIMER1 = 0xf9934def, TIMER2 = 0x1 TIMER1 = 0xfa1ccf0b, TIMER2 = 0x1 TIMER1 = 0xfaa65039, TIMER2 = 0x1 TIMER1 = 0xfb2fd15b, TIMER2 = 0x1 TIMER1 = 0xfbb95283, TIMER2 = 0x1 TIMER1 = 0xfc42d3b1, TIMER2 = 0x1 TIMER1 = 0xfccc54d9, TIMER2 = 0x1 TIMER1 = 0xfd55d601, TIMER2 = 0x1 TIMER1 = 0xfddf5729, TIMER2 = 0x1 TIMER1 = 0xfe68d851, TIMER2 = 0x1 TIMER1 = 0xfef2597f, TIMER2 = 0x1 TIMER1 = 0xff7bdaa1, TIMER2 = 0x1 TIMER1 = 0xf0055bc9, TIMER2 = 0x1 --------------------> 7th OverFlow TIMER1 = 0xf08edceb, TIMER2 = 0x1 TIMER1 = 0xf1185e1f, TIMER2 = 0x1 TIMER1 = 0xf1a1df47, TIMER2 = 0x1 TIMER1 = 0xf22b606f, TIMER2 = 0x1 TIMER1 = 0xf2b4e191, TIMER2 = 0x1 TIMER1 = 0xf33e62bf, TIMER2 = 0x1 TIMER1 = 0xf3c7e3e7, TIMER2 = 0x1 TIMER1 = 0xf4516509, TIMER2 = 0x1 TIMER1 = 0xf4dae631, TIMER2 = 0x1 TIMER1 = 0xf5646753, TIMER2 = 0x1 TIMER1 = 0xf5ede87b, TIMER2 = 0x1 TIMER1 = 0xf67769a3, TIMER2 = 0x1 TIMER1 = 0xf700eac5, TIMER2 = 0x1 TIMER1 = 0xf78a6bf3, TIMER2 = 0x1 TIMER1 = 0xf813ed1b, TIMER2 = 0x1 TIMER1 = 0xf89d6e43, TIMER2 = 0x1 TIMER1 = 0xf926ef6b, TIMER2 = 0x1 TIMER1 = 0xf9b0708d, TIMER2 = 0x1 TIMER1 = 0xfa39f1a9, TIMER2 = 0x1 TIMER1 = 0xfac372cb, TIMER2 = 0x1 TIMER1 = 0xfb4cf3e7, TIMER2 = 0x1 TIMER1 = 0xfbd67515, TIMER2 = 0x1 TIMER1 = 0xfc5ff637, TIMER2 = 0x1 TIMER1 = 0xfce9775f, TIMER2 = 0x1 TIMER1 = 0xfd72f88d, TIMER2 = 0x1 TIMER1 = 0xfdfc79b5, TIMER2 = 0x1 TIMER1 = 0xfe85fae9, TIMER2 = 0x1 TIMER1 = 0xff0f7c11, TIMER2 = 0x1 TIMER1 = 0xff98fd39, TIMER2 = 0x1 TIMER1 = 0xf0227e61, TIMER2 = 0x1 --------------------> 8th OverFlow TIMER1 = 0xf0abff89, TIMER2 = 0x1 TIMER1 = 0xf13580ab, TIMER2 = 0x1 TIMER1 = 0xf1bf01df, TIMER2 = 0x1 TIMER1 = 0xf2488301, TIMER2 = 0x1 TIMER1 = 0xf2d20429, TIMER2 = 0x1 TIMER1 = 0xf35b854b, TIMER2 = 0x1 TIMER1 = 0xf3e5067f, TIMER2 = 0x1 TIMER1 = 0xf46e87a7, TIMER2 = 0x1 TIMER1 = 0xf4f808c9, TIMER2 = 0x1 TIMER1 = 0xf58189f1, TIMER2 = 0x1 TIMER1 = 0xf60b0b0d, TIMER2 = 0x1 TIMER1 = 0xf6948c35, TIMER2 = 0x1 TIMER1 = 0xf71e0d5d, TIMER2 = 0x1 TIMER1 = 0xf7a78e85, TIMER2 = 0x1 TIMER1 = 0xf8310fa7, TIMER2 = 0x1 TIMER1 = 0xf8ba90cf, TIMER2 = 0x1 TIMER1 = 0xf94411f7, TIMER2 = 0x1 TIMER1 = 0xf9cd931f, TIMER2 = 0x1 TIMER1 = 0xfa571447, TIMER2 = 0x1 TIMER1 = 0xfae09569, TIMER2 = 0x1 TIMER1 = 0xfb6a1697, TIMER2 = 0x1 TIMER1 = 0xfbf397c5, TIMER2 = 0x1 TIMER1 = 0xfc7d18e7, TIMER2 = 0x1 TIMER1 = 0xfd069a09, TIMER2 = 0x1 TIMER1 = 0xfd901b2b, TIMER2 = 0x1 TIMER1 = 0xfe199c47, TIMER2 = 0x1 TIMER1 = 0xfea31d75, TIMER2 = 0x1 TIMER1 = 0xff2c9e97, TIMER2 = 0x1 TIMER1 = 0xffb61fbf, TIMER2 = 0x1 TIMER1 = 0xf03fa0ed, TIMER2 = 0x4 --------------------> 9th OverFlow TIMER1 = 0xf0c92215, TIMER2 = 0x4 TIMER1 = 0xf152a33d, TIMER2 = 0x4 TIMER1 = 0xf1dc2465, TIMER2 = 0x4 TIMER1 = 0xf265a587, TIMER2 = 0x4 TIMER1 = 0xf2ef26bb, TIMER2 = 0x4 TIMER1 = 0xf378a7dd, TIMER2 = 0x4 TIMER1 = 0xf4022905, TIMER2 = 0x4 TIMER1 = 0xf48baa27, TIMER2 = 0x4 TIMER1 = 0xf5152b5b, TIMER2 = 0x4 TIMER1 = 0xf59eac83, TIMER2 = 0x4 TIMER1 = 0xf6282da5, TIMER2 = 0x4 TIMER1 = 0xf6b1aecd, TIMER2 = 0x4 TIMER1 = 0xf73b2fe9, TIMER2 = 0x4 TIMER1 = 0xf7c4b111, TIMER2 = 0x4 TIMER1 = 0xf84e3239, TIMER2 = 0x4 TIMER1 = 0xf8d7b361, TIMER2 = 0x4 TIMER1 = 0xf961348f, TIMER2 = 0x4 TIMER1 = 0xf9eab5b7, TIMER2 = 0x4 TIMER1 = 0xfa7436df, TIMER2 = 0x4 TIMER1 = 0xfafdb801, TIMER2 = 0x4 TIMER1 = 0xfb87392f, TIMER2 = 0x4 TIMER1 = 0xfc10ba57, TIMER2 = 0x4 TIMER1 = 0xfc9a3b7f, TIMER2 = 0x4 TIMER1 = 0xfd23bca7, TIMER2 = 0x4 TIMER1 = 0xfdad3dc9, TIMER2 = 0x4 TIMER1 = 0xfe36bef7, TIMER2 = 0x4 TIMER1 = 0xfec04025, TIMER2 = 0x4 TIMER1 = 0xff49c141, TIMER2 = 0x4 TIMER1 = 0xffd34269, TIMER2 = 0x4 TIMER1 = 0xf05cc38b, TIMER2 = 0x4 --------------------> 10th OverFlow TIMER1 = 0xf0e644b3, TIMER2 = 0x4 TIMER1 = 0xf16fc5db, TIMER2 = 0x4 TIMER1 = 0xf1f94703, TIMER2 = 0x4 TIMER1 = 0xf282c82b, TIMER2 = 0x4 TIMER1 = 0xf30c4959, TIMER2 = 0x4 TIMER1 = 0xf395ca7b, TIMER2 = 0x4 TIMER1 = 0xf41f4ba3, TIMER2 = 0x4 TIMER1 = 0xf4a8ccd1, TIMER2 = 0x4 TIMER1 = 0xf5324df9, TIMER2 = 0x4 TIMER1 = 0xf5bbcf21, TIMER2 = 0x4 TIMER1 = 0xf6455049, TIMER2 = 0x4 TIMER1 = 0xf6ced16b, TIMER2 = 0x4 TIMER1 = 0xf7585287, TIMER2 = 0x4 TIMER1 = 0xf7e1d3bb, TIMER2 = 0x4 TIMER1 = 0xf86b54dd, TIMER2 = 0x4 TIMER1 = 0xf8f4d605, TIMER2 = 0x4 TIMER1 = 0xf97e572d, TIMER2 = 0x4 TIMER1 = 0xfa07d849, TIMER2 = 0x4 TIMER1 = 0xfa915971, TIMER2 = 0x4 TIMER1 = 0xfb1ada99, TIMER2 = 0x4 TIMER1 = 0xfba45bc1, TIMER2 = 0x4 TIMER1 = 0xfc2ddcef, TIMER2 = 0x4 TIMER1 = 0xfcb75e17, TIMER2 = 0x4 TIMER1 = 0xfd40df3f, TIMER2 = 0x4 TIMER1 = 0xfdca6061, TIMER2 = 0x4 TIMER1 = 0xfe53e18f, TIMER2 = 0x4 TIMER1 = 0xfedd62b7, TIMER2 = 0x4 TIMER1 = 0xff66e3df, TIMER2 = 0x4 TIMER1 = 0xfff06507, TIMER2 = 0x4 TIMER1 = 0xf079e629, TIMER2 = 0x4 --------------------> 11th OverFlow TIMER1 = 0xf1036757, TIMER2 = 0x4 TIMER1 = 0xf18ce885, TIMER2 = 0x4 TIMER1 = 0xf21669a1, TIMER2 = 0x4 TIMER1 = 0xf29feac9, TIMER2 = 0x4 TIMER1 = 0xf3296beb, TIMER2 = 0x4 TIMER1 = 0xf3b2ed07, TIMER2 = 0x4 TIMER1 = 0xf43c6e35, TIMER2 = 0x4 TIMER1 = 0xf4c5ef57, TIMER2 = 0x4 TIMER1 = 0xf54f707f, TIMER2 = 0x4 TIMER1 = 0xf5d8f1ad, TIMER2 = 0x4 TIMER1 = 0xf66272d5, TIMER2 = 0x4 TIMER1 = 0xf6ebf3fd, TIMER2 = 0x4 TIMER1 = 0xf7757525, TIMER2 = 0x4 TIMER1 = 0xf7fef647, TIMER2 = 0x4 TIMER1 = 0xf8887775, TIMER2 = 0x4 TIMER1 = 0xf911f89d, TIMER2 = 0x4 TIMER1 = 0xf99b79cb, TIMER2 = 0x4 TIMER1 = 0xfa24fae7, TIMER2 = 0x4 TIMER1 = 0xfaae7c1b, TIMER2 = 0x4 TIMER1 = 0xfb37fd3d, TIMER2 = 0x4 TIMER1 = 0xfbc17e65, TIMER2 = 0x4 TIMER1 = 0xfc4aff8d, TIMER2 = 0x4 TIMER1 = 0xfcd480b5, TIMER2 = 0x4 TIMER1 = 0xfd5e01dd, TIMER2 = 0x4 TIMER1 = 0xfde782ff, TIMER2 = 0x4 TIMER1 = 0xfe71042d, TIMER2 = 0x4 TIMER1 = 0xfefa8555, TIMER2 = 0x4 TIMER1 = 0xff84067d, TIMER2 = 0x4 TIMER1 = 0xf00d87a5, TIMER2 = 0x7 --------------------> 12th OverFlow TIMER1 = 0xf09708c7, TIMER2 = 0x7 TIMER1 = 0xf12089e3, TIMER2 = 0x7 TIMER1 = 0xf1aa0b05, TIMER2 = 0x7 TIMER1 = 0xf2338c33, TIMER2 = 0x7 TIMER1 = 0xf2bd0d61, TIMER2 = 0x7 TIMER1 = 0xf3468e7d, TIMER2 = 0x7 TIMER1 = 0xf3d00fa5, TIMER2 = 0x7 TIMER1 = 0xf45990c7, TIMER2 = 0x7 TIMER1 = 0xf4e311ef, TIMER2 = 0x7 TIMER1 = 0xf56c9317, TIMER2 = 0x7 TIMER1 = 0xf5f6143f, TIMER2 = 0x7 TIMER1 = 0xf67f9567, TIMER2 = 0x7 TIMER1 = 0xf7091695, TIMER2 = 0x7 TIMER1 = 0xf79297b7, TIMER2 = 0x7
From the above logs:
1) It seems to take around 6 overflows in TIMER 1 to get the 1st increment in TIMER2
2) After the 1st increment, the TIMER2 gets incremented 3 timers after every 3rd overflow of TIMER 1
Whereas, the expectation is:
TINMER2 should increment at every overflow of TIMER 1
How do we implement the cascaded timer feature? Is there anything wrong with the above implementation?