This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: DSP Devlopment: run a pdk example on a custom board

Part Number: AM5748

Tool/software:

Hi,

I need to know the steps we need to follow so as to run a pdk example on a custom board from the linux user space.

I have build the pdk library and also build the example applications for a McSPI loop back application.

Here I need to set up a UART and SPI for a custom board.

What are the changes we need to follow to make it working on a custom board. The board I am using is Critical Link AM57F SoM based board.www.criticallink.com/.../