Other Parts Discussed in Thread: AM625
Tool/software:
Dear TI.
I'd like to verify Main MCAN function with SK-AM62B-P1
According to below link, it seems that I could enable Main MCAN in SK-AM62B-P1
- SK-AM62B-P1: Unable to access can on the EVM
In the SK_AM62B-P user manaual, it seems that MCAN0_RX and MCAN0_TX are exposed via Pin User Expansion Connector.
But the description is a bit vague since there was no MCAN0 like below.
| Pin No | Soc Ball | Net Name | Pin Multiplexed Signals
| 8 | E15 | EXP_UART5_TXD | UART5_TXD/ TIMER_IO3/ SYNC3_OUT/UART1_RIn/ EQEP2_S/ PR0_UART0_TXD/GPIO1_25/ MCASP2_AXR1/ EHRPWM_TZn_IN4
In AM625 datasheet, there is MCAN0_RX at E15.
Could you let me know whether MCAN0_RX and MCAN0_TX are exposed or not via Pin User Expansion Connector. ?
If they are exposed, can I verify MCAN function with below connection ?
[1'st SK_AM62B-P] [2nd SK_AM62B-P]
MCAN0_RX --------------------- MCAN0_TX
MCAN0_TX --------------------- MCAN0_RX
BR
Jace