Other Parts Discussed in Thread: SYSBIOS
I'm using Code Composer Studio 4 to experiment with a Stellaris board and I've run into a snag using SYS/BIOS and timers.
I can create a new project with any of the sys/bios examples and it compiles, links and runs on the board just fine. But I need to make an example for timers. So I add the following:
#include <ti/sysbios/hal/Timer.h>
int main()
{
Timer_Handle t = Timer_create(1, func, NULL, NULL);
....
}
The error I'm getting when I build is : undefined symbol ti_sysbios_hal_Timer_Object__create__S
So I looked in hal/Timer.h and I see that one of the inline functions is
calling ti_sysbios_dal_Timer_Object__create__S. The problem is, this
doesn't seem to be actually defined anywhere. Does anybody know how I can get this to build?