Hello,
I have been testing on pcie with TMDXEVMPCI AMC-PCIe adapter card. I have followed the instruction on MCSDK 2.00.02.14 - the PCIe Boot Example that came with MCSDK 2.00.02.14 release , mcsdk_2_00_02_14\tools\boot_loader\examples\pcie\docs\README.pdf but my Linux PC as well as Windows PC don't detect the c6678 card at all. I have checked it on Ubuntu 10.04 using lspci as well as pciedemo kernel module. The card has not been detected.
Also I double checked the SW setting and all setting look fine. My development environment are below.
- Host PC : Linux Ubuntu 10.04 64bit on AMD 64bit PC, Windows XP 32bit on AMD 64bit PC
- Target board : TMS320C6678 LE
- TMDXEVMPCI AMC to PCIe adaptor module
- MCSDK v2.00.02.14
I believe that I miss something. Please let me know what I miss. Thank you for help in advance.