Tool/software:
Are there any examples for USB and Ethernet available?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jim,
Can you elaborate more on what examples are you looking for? Are you enquiring about booting via USB/Ethernet? Also are you planning to use Linux as the HLOS?
Best Regards,
Suren
If there were any examples we could use through CCS to verify functionality (at this point) that would be great! If I need to modify an existing Image, that may work, as well. I've used "tisdk-default-image-am62xx-lp-evm.wic.xz" on the development board but we'd be running software on a custom board.
Hi Jim,
Can you create two separate threads one for USB and other for Ethernet, to better support your query.
Also, Are you planning to use Linux, but there is no Linux example which can run in CCS.
Please look at our AM62x Academy:
Best Regards,
Suren
OK! I will create two threads. Also, we don't need to use Linux if there is an alternative. Whatever operating system allows us to quickly test the functionality will do.
We do want to show we can boot the system so at a later phase, it would be beneficial to boot an image (Linux) from an SD Card, for instance. The image could be very minimal - only 2 Ethernet and One USB. (and one UART)
Thanks Jim.
I am going to close this thread and assign each of the other threads to our Subject Matter Experts for further support.
Best Regards,
Suren